cancel
Showing results for 
Search instead for 
Did you mean: 

CMSIS DSP

cbenson
Associate
Posted on October 30, 2015 at 21:05

I am trying to implement an FFT on Nucleo-L053R8. I am using System Workbench and STM32CubeMX, on Windows 7 64. Adding a function like arm_rfft_init_q15, causes the program size to become so large as to no longer fit in the STM32L053. Is this a consequence of having to load the floating point libraries from ARM_MATH? I believe I have the linker set to only load referenced code. May I am missing something. I could switch to a CPU with a FPU, but this is not a high performance instrument, I would like to avoid overkill.

Regards,

Corky

#stm32l0-dsp-cmsis
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on October 30, 2015 at 21:14

The source to the DSP library is available. You should be able to look at the size of the object files. The .MAP should be able to provide you with a break-down of the contribution of each function pulled into the image, at least Keil does this.

The Cortex-M0 has the smallest instruction set, objects are going to be some what bigger than those for the M3/M4 parts as more instructions are needed to perform the same tasks.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..