STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! i2s 44khz wav file not playing properly

I am trying to read a file from sdcard using fatfs and sdio and output it to i2s8khz, 16bit is output wellBut 44khz, 16bit file is not played properlyThe mcu is using stm32h743dma is using circular mode and the source is belowThank you#define AUDIO_B...

eunoia by Associate II
  • 988 Views
  • 1 replies
  • 1 kudos

Resolved! GPIO pin max current input (sink)

I want to use led with following connection and i remember that I've seen this application somewhere on the Internet:3V3 - LED - RESISTOR - STM32 PINI've seen the max total current output of MCU then is there any max total input current of MCU?

yonggeon by Associate II
  • 3383 Views
  • 7 replies
  • 3 kudos

IWDG Doesn't Reset Without Refreshing with F103RC

Hi,I am trying to use IWDG to function as a 5s timer, IWDG is reloaded every second. In order to test the functionality, I just activated it with default parameters of PRESCALER=4 RELOAD VALUE=4095, and I did nothing else (no refreshing the timer), w...

Chao_0-1736418375886.png Chao_1-1736418396524.png
Chao by Senior II
  • 2255 Views
  • 6 replies
  • 0 kudos

How send answer on UDP server ?

Hello,I created UDP server with LwIP stack on STM32F407.I tried example udp_echo _server. It works.Now I need send from server my own answer data in callback function.The program hangs in callback function.void udp_echoserver_receive_callback(void *a...

Peko by Associate III
  • 1138 Views
  • 1 replies
  • 0 kudos

Resolved! STM32 Nucleo- L4A6ZG differential ADC input Error.

Hi there. I am testing my circuit with a 3.3V sine wave that has a 1.65V DC offset. PC01 has the Signal InputPC02 has the 1.65V.Looking at the output file from the ADC, I am not getting the total signal. 0-4096. My wave is between 1000 and 3000 appro...

nafis by Associate II
  • 2359 Views
  • 4 replies
  • 0 kudos

Resolved! I2S weird bit shift problem

Hi,I'm getting a problem in my project, where I tried to create a loopback between I2S3 and I2S4 on STM32F411 Disco.It seems that only the least significant bit of 16-bit packets is somehow shifted to the next packet. The rest of the transmission is ...

baator025 by Associate III
  • 11305 Views
  • 31 replies
  • 1 kudos

Potential memory leak in SPI HAL for STM32H753

Configuring SPI for 24 bit data frames and receiving single data frames via HAL_SPI_Receive_IT (which redirects to HAL_SPI_TransmitReceive_IT() in case bidirectional transfer is enabled), hspi->RxXferCount and hspi->RxXferSize are both set to the val...

MNagl.1 by Associate II
  • 1316 Views
  • 1 replies
  • 0 kudos

Resolved! General Purpose Timer as Wakeup

Hi guys, im initializing a low/ultra low power project and i will use the STM32C011J4M6, i need to know if a general purpose timer like the TIM14 can wakeup the microcontroller in the low power modes (sleep, stop, etc).I was reading the datasheet (i ...

Resolved! SPI vs GPIO - Alternate Functions (AF)

@Tesla DeLorean Hi! Thank you for helping me with the BOOTING process. However, I have a question about the peripherals. I am planning to control a TFT screen that requires 40 pins and RGB protocol. At first, I was planning to choose random GPIOs to ...

STM32U5 - Enable MDF use ADC1 as data source

Hello, I have further questions related to ADC1 and MDF. The solution solved this case: ADC1 with one single input channel.  How about multiple input channels are connected to ADC1 of STM32U585?  I use 4x analog inputs as example, they are connected ...

YN15054_3-1736492606790.png
YN15054 by Associate
  • 1350 Views
  • 1 replies
  • 0 kudos