STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PA2 pin goes low on power up for no reason.

Hello to everyonesIn a project where I used the STM32G0B1RTC6 MCU I have the following problem:The PA2 pin used as uart2 TX sometimes goes low at power on and stays there forevereven if I try to reset the CPU again. If it is configured regularly then...

10-Bit DVP (DCMI) input to DVI/HDMI output

Hi,Our team is working on a board that should provide the ability to stream a video from OmniVisions' OV6946 tiny CMOS camera module to a monitor with DVI port https://www.ovt.com/sensors/OV6946We are planning to use OV426 as a convertor into a parra...

jjjj by Associate
  • 4658 Views
  • 1 replies
  • 1 kudos

Strange ADC issue in STM32G491

Hi,I have a very strange ADC issue which I am unable to find the root cause to. The symptom is as follows;While performing ADC readings to ADC1 IN1 and ADC2 IN1 consecutively, the readings sometimes differ by more than 32 ADC counts. I perform this c...

macbum by Associate II
  • 4113 Views
  • 10 replies
  • 2 kudos

Resolved! STM32G070CB v1.2 bootloader issues with some commands

Hello, I'm trying to communicate with a STM32G070CBT6 bootloader, with mixed success. I've forced the chip into bootloader mode by writing a 0xDBFFE1AA to the FLASH option register (by default it was DFFFE1AA). I've verified that this value "stuck", ...

sgordon777_0-1736617801172.png sgordon777_1-1736618016555.png

offset and linearity calibration

Hello,I'm working with the offset and linearity calibration on an STMH755.  My board will run the full calibration at production, save off the resulting offset and linearity calibration constants, and then retrieve and apply them at any new restarts ...

R_DSP by Associate II
  • 1818 Views
  • 2 replies
  • 2 kudos