STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cube Clock Confgration bug

Posted on May 19, 2016 at 09:00Dear all ST staffs, I found a bug about clock configuration for F429-NUCLEO in cubeMX. I want you to fix this problem. To reproduce the bug, please make a new F429-NUCLEO project, and choose HSI as clock source. The fr...

STM32F3/F7 SPI with DMA implementation

Posted on May 24, 2016 at 09:22Hello,I want to use SPI to transmit/receive data on two board (F3 vs F7), that using SPI/DMA. But I don't know how to implement.I have seen SPI/DMA examples in STM32Cube Firmware packages but it seem transmit/receiver ...

STM32F105 - Correct method for ADC Calibration?

Posted on May 24, 2016 at 03:30Hello,It looks like there is a discrepancy between the StdPeriphLib example programs and the Reference Manual regarding the ADC calibration.  Which is the correct method?In the RM0008 Reference Manual, Rev 14, Section ...

jfolsom by Associate II
  • 964 Views
  • 0 replies
  • 0 kudos

CAN message being sent only once

Posted on May 21, 2016 at 18:17 Hi, I m using STM32F103 Nucleo board and keil compiler. I m using HAL_CAN stack. I configured filter in mask mode and set to receive all messages. Mode : Loopback mode speed : 250 kbps ID : stand...

SS.Sagar by Associate III
  • 1143 Views
  • 2 replies
  • 0 kudos

STM32 HAL UART Receive Issues

Posted on May 17, 2016 at 22:02 Hi all, I have recently run into an issue trying to use the HAL_UART_Receieve() function which comes with the HAL library. I am using the Nucle-F303RE board, which uses the STM32F303RE microcontroller. I wa...

ifarah by Associate
  • 1440 Views
  • 1 replies
  • 0 kudos

CubeMX problem....

Posted on May 20, 2016 at 23:00I'm using the wakeup interrupt from the RTC, but I don't want it active until certain conditions are present.But I have no choice, either I disable it in Cube and get no stubs for interrupts and no definition, or I ena...

mattreed9 by Associate III
  • 1952 Views
  • 3 replies
  • 0 kudos

AN2824, Optimised I2C - applicable to STM32F411 ?

Posted on May 11, 2016 at 12:26AN2824: Application note - STM32F10xxx I2C optimized examples''This application note applies to STM32F101xx and STM32F103xx medium, high and XL density microcontrollers, STM32F105/107xx connectivity line and STM32F100x...

cubemx USB on STM32F3Discovery

Posted on May 21, 2016 at 22:39I'm having some difficulty getting the default HID or VCOM projects to run properly.  I've set the HSI input and let the clock configuration do its thing.   The projects compile fine, but when I try to run them on a Ma...

Device information at runtime

Posted on May 23, 2016 at 14:00Hi,I need to distinguish between diffrent types of STM32 devices during runtime .Specifically between F2 and F4 and their sub types. Can this information be parssed from the Unique ID?Is there a way to get at runtime t...

ari_v2 by Senior
  • 745 Views
  • 2 replies
  • 0 kudos