STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

howto reset stm32 by software properly

Posted on May 23, 2016 at 12:15Hello, i have an application that should restart from time to time (bootloader). Currently I do NVIC_SystemReset(). But it seems that only the CortexCore and not the internal peripherals are reset. Some of the CubeMx F...

taraben by Senior
  • 1240 Views
  • 1 replies
  • 1 kudos

Interrupts during flash programming

Posted on May 02, 2016 at 08:23While programming the flash memory cannot provide instructions to the processor for execution. So you can only run programs from cache (which you processor doesn't have) or RAM. I expect that your code writes a group o...

STM32F103 DMA transfer trigger with output compare

Posted on May 21, 2016 at 03:46 Hi, I am trying to configure timer 1 channel 3 to output a varying signal in output compare toggle mode and driving the CCR with DMA1 channel 5. Thus far I can get the DMA transfer triggering using the TIM_DMA_...

CubeMX: SD_Card SPI

Posted on May 23, 2016 at 08:35How can I use the SPI to write to SD_Card (with HAL lib.) because CubeMx forces me to use SDIO which I have no access to it.is there is an HAL example using SPI to drive the SD card?

Mixed Thumb and ARM modes in .init section hard fault

Posted on May 23, 2016 at 01:07I have a 5 liner 'c' code to copy a module into ccmram which I put into the .init section which works fine. However, immediately after this function, libc_array_init() is called which results in a hard fault. I think t...

STM32F070 Breakout board

Posted on October 24, 2015 at 20:23I designed the following circuit to interface an STM32F070 Micro for a project I'm working on. I was hoping to get some feedback if I was doing everything the right way/will it work , before I order the PCB and BOM...

0690X00000605GxQAI.png
monta by Associate II
  • 1504 Views
  • 2 replies
  • 0 kudos

read and write SRAM internal

Posted on May 21, 2016 at 12:11I would read and write about 10kB of 64kB SRAM internal with STM32F103ZE.This micro have the SRAM at start address 0x20000000.How can I use and save the area of RAM, sure this area isn't changed in real time during the...

vbruno1 by Associate III
  • 781 Views
  • 1 replies
  • 0 kudos

STM32F103C8 - PLL Ready Flag never sets

Posted on May 13, 2016 at 06:55 I am trying to set PLL as my system clock source upon startup of my microcontroller, STM32f103 I have commented all the defines in my system_stm32f10x.c 1. white-space: inherit;''> /* #define SYSCLK_FREQ_HSE H...

STM32CubeMX v4.14.0 bug - NVIC fixed priority (0,0)

Posted on May 19, 2016 at 23:09In linux STM32CubeMX v4.14.0 doesn't allow NVIC priority changing. Under the Configuration tab / NVIC Settings after enabling an interrupt the Priority and Sub Priority fields are still read-only and fixed at 0,0 so al...

emil by Associate II
  • 1889 Views
  • 2 replies
  • 0 kudos