STM32L152 comparator triggers timer
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-11-12 2:30 AM
Posted on November 12, 2015 at 11:30
Is it possible to trigger any timer by comparator output in stm32l152? I want to configure timer to one pulse mode and i want to trigger it by comparator output. I have studied manual carefully, but I still don't know if it is possible.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-12-03 2:41 AM
Posted on December 03, 2015 at 11:41
Hi legierski.michal,
Please refer to the description of OUTSEL bits in COMP_CSR register to know the Timers that are connected to comparator output. Only TIM2/3/4/10 can be used: Bits 23:21 OUTSEL: Comparator 2 output selectionThese bits are written by software to connect the output of COMP2 to a selected timer input.
000 = TIM2 Input Capture 4
001 = TIM2 OCREF_CLR
010 = TIM3 Input Capture 4
011 = TIM3 OCREF_CLR
100 = TIM4 Input Capture 4
101 = TIM4 OCREF_CLR
110 = TIM10 Input Capture 1
111 = no redirection-Mayla-
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.