STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Limitation with Read protection active with stm32f105rb

Posted on June 15, 2016 at 16:03Hi, I made a loader with usb STM32F105 and working properly. When I active the read protection bit, the loader not erase the pages. The security bit is on and of course, I can not debug and find where is the problem. ...

Marco1 by Associate II
  • 648 Views
  • 1 replies
  • 0 kudos

Problem with RTC and LPTIM interrupt in STOP Mode

Posted on June 14, 2016 at 16:31I am using NUCLEO-L11K4 board for my low power monitor project. I want to wake up board periodically every 5 minutes and send message center. Meanwhile i want to wake up the board with external interrupt in the case o...

Receiving register address byte with STM32F407 as I2C slave

Posted on June 15, 2016 at 00:58 Hi I have written a small proeject where I have set up an STM32F407 on a discovery board as an I2C slave, and I'm pleased to say that it is mostly working. The problem I have is that when I send the follo...

AJE by Associate II
  • 1078 Views
  • 2 replies
  • 0 kudos

UDP packet receive problem

Posted on August 24, 2015 at 12:59Hi all, I'm using UDP Echo client code example in STM32F217xx.I can send the custom buffer...ok but I can't receive udp packets from PC. I have a VS code that can generate UDP test packets as well... I use the udp_r...

borzoo by Associate
  • 2443 Views
  • 3 replies
  • 0 kudos

STM32F4 DISCO Print to /dev/tty

Posted on June 10, 2016 at 19:20I have seen several people use the ''cat /dev/USB<some number>'' can get information from the board printed to a Linux terminal via USB cable. I have followed a few guides (http://www.carminenoviello.com/2015/03/02/ho...

audio crosstalk/ringing (solution)

Posted on June 14, 2016 at 17:09Tried to post a reply to my older posting asking about this but it says ''page not found'' hence the new post.  I think I found the issue.  Down in the bowels of WM8994 setup the driver is setting registers 0x29 and 0...

dennis by Associate II
  • 1102 Views
  • 1 replies
  • 0 kudos

STM32F070CBT6 UART Bootloader does not work

Posted on June 13, 2016 at 20:32Hi, I have evidence that the UART embedded bootloader of the STM32F070CBT6 does not work. Is this expected ? I have tried the boot sequence with other STM32 variants for years, and I cannot find any written explanatio...

usrfaqr by Associate
  • 1300 Views
  • 2 replies
  • 0 kudos

STM32F429 I2C for SMBUS

Posted on June 12, 2016 at 05:29Hey folks, I am trying to implement an SMBUS protocol on an STM32F29 board using the HAL-I2C drivers. Main purpose is to be able to read a MLX90614 temp sensor and report the output to the screen. I am getting some od...

moritz by Associate
  • 1084 Views
  • 1 replies
  • 0 kudos