STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO speed settings

Posted on June 16, 2016 at 08:28Hi. I would like to ask if speed setting of a pin in GPIO->OSPEEDR register is relevant also if a pin is configured in input/alternate mode? Or is this setting relevant only for output mode? I am asking specifically f...

matic by Associate III
  • 2354 Views
  • 1 replies
  • 0 kudos

F103, F401, F407 USB code replace

Posted on June 15, 2016 at 22:41Hi. I found this project : https://github.com/jpbarraca/LogicAlNucleo This code is for NucleoF401RE board, which costs about $20. I have cheap chinese board with STM32F103C8T6, resources looks enought, but code not w...

tuxcnc by Associate
  • 2201 Views
  • 3 replies
  • 0 kudos

Problems with cube implementation of get/set for RTC

Posted on June 16, 2016 at 00:49The cube hal code for getting and setting the time/date have some significant issues -- at the very least the documentation is woefully inadequate.The fundamental issue is that setting (getting) time/date requires two...

Specifications for the F429 DISCO LCD available?

Posted on October 10, 2013 at 15:03Hello, are specifications and command descriptions for the LCD Display on the F429 Disco available? It is a SF-TC240T-9370-T type display. Google only brings up information for the SF-TC240T-9229A2-T that doesn't h...

STM32F072xx USB Hardware

Posted on June 14, 2016 at 22:54Hello,Where can I find info on hardware needed to run USB to my STM32F072CB?  I found the reference design and read hardware getting started.  Neither specify how to get USB levels down from 5V to uC VDD.  5V can't go...

jezell by Associate
  • 2123 Views
  • 4 replies
  • 0 kudos

three_input_capture_xor_gate reading on stm32f429i_discovery

Posted on June 15, 2016 at 18:33Hello, We would like to read hal sensor outputs(H1,H2,H3) of bldc motor by xor gate of TIM4 channels. We select SLAVE mode for RESET MODE to read number of squarewave of xor gate outputs of TIMER4 but it does not wor...

bhakan by Associate II
  • 1235 Views
  • 1 replies
  • 0 kudos

Install u-boot on stm32f4 discovery board

Posted on June 15, 2016 at 17:44Hello guys, I'm trying to install u-boot on my development board STM32F407 . After loading the binary image, the UART1 interface does not work . I'm using the version available from the website emcraft for the board S...

rs23 by Associate II
  • 949 Views
  • 1 replies
  • 0 kudos

replace STM32F405 with STM32F415

Posted on June 14, 2016 at 21:16Hi all,I have a design based on the  STM32F405  working, I would now like to try out the  STM32F415, is it the case that  on the hardware side I can just replace the  STM32F405  on PCB with the  STM32F415 - given that...

kweisi50 by Associate II
  • 917 Views
  • 2 replies
  • 0 kudos

STM32 part numbering ''Software option''?

Posted on June 15, 2016 at 08:26Hi, In STM32F105xx datasheet, in part numbering section, it has an option named ''Software option'', and it has two options: internal code or black. What does it mean? #!stm32 #part-numbering

0690X00000605PoQAI.png