STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to clear SPI TX Buffer

Posted on January 02, 2012 at 04:06I am using STM32F103 MPU.I set the board as SPI Slave and uses DMA to receive and send data.Most of time Command comes from Master and Slave responses.So I made code to wait for receiving Command from Master. Once ...

DMA to GPIO output pins

Posted on June 28, 2016 at 17:39I wish to transfer a large array of data to 8 output pins that are all on the same port. E.g. a 500 element 8bit array where each bit of each element represents the pin status.So 500 independent transfers to the port ...

usart baud rate

Posted on June 30, 2016 at 12:38hi i wanna connect stm32f407discovery board to stm32f429 via uart communication. how can I calculate the closest baud rate to 5Mbps for these 2 board? I use following cod and it work but I want to be sure about minimu...

sanaz by Associate II
  • 1331 Views
  • 2 replies
  • 0 kudos

fsmc external adc

Posted on June 30, 2016 at 13:14i want to make low cost oscilloscope i want the maximum speed can i work with  external adc  using stm32f4 what is best dcmi or fsmc and can change  dcmi or fsmc  clock out frequency through mcu running.  https://www...

elec_st by Associate III
  • 1125 Views
  • 1 replies
  • 0 kudos

vector table relocation VTOR

Posted on June 29, 2016 at 15:11Hi there, I'm implementing a bootloader. And have created an application vector table that is different to the bootloader vector table Boot Vectors at 0x08000000 App Vectors  at 0x08010400 volatile const void (*vector...

controller SPI Chip select hardware configurations

Posted on June 30, 2016 at 11:53Hi,i am designing one sensor motion board using STM32411CC for which we wanted to connect four 6 axis inertial sensors to STM32F411CC controller( 48 pin package) using SPI bus and the selected controller having only t...

How to use Cube to configure LCD on 469i-Disco Board?

Posted on June 29, 2016 at 22:09Are there any examples or documentation to describe how to configure Cube to run the LCD and touchscreen on the 469i_Disco board? I'm finding this to be a monumental task since the 469i-Disco uses DMA2D, FMC/SDRAM1, I...

Recovering from an aborted full flash erase

Posted on June 28, 2016 at 08:29I initiated a change from RDP level 1 to RDP level 0, which in turn initiated a full flash erase.  But before that process completed I pull the power on the chip.  Now dfu-util refuses to load new code, saying:dfu-uti...

ron2399 by Associate II
  • 2408 Views
  • 4 replies
  • 0 kudos