STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CRC multithreading

Posted on July 01, 2016 at 10:45Good day. In my program i use CAN interface. I send and receive messages (consist of few CAN packs) with crc. When i receive the CAN pack i put it into buffer and when the message complete i calculate it crc.Transm...

STM32 F0 - leaving dfu mode

Posted on June 30, 2016 at 16:49Hello,I have a board with F072, BOOT 0 pin is low.When I use ''Leave DFU mode'' (Dfuse Demo 3.0.5), board left DFU mode but the application is not restarted.  Content of flash memory at address 0x00000000 and at addre...

SPI slave TX FIFO clearing....

Posted on June 30, 2016 at 16:20I have an SPI slave. The master may request data at a faster pace than I can handle in software, so I've set up DMA. I've prepared a buffer etc. Now after one transfer, I get an interrupt of the DMA having finished (i...

Schematics for SPDIF OUT circuit after STM32F7

Posted on June 25, 2016 at 09:20Hello, I'm looking for information about the circuits to add to a STM32F7 Nucleo board to build an operational SPDIF output. I tried to find the information in the STM32 reference document, but could not find the inf...

jmf1 by Senior
  • 2443 Views
  • 5 replies
  • 0 kudos

Code only executes when semihosting

Posted on June 28, 2016 at 21:11I have a STM32F4 Discovery board. I have GDB connected to OpenOCD and when I run my program on GDB it executes perfectly. When I disconnect the board and program it via ST-Link nothing happens. I tried and older progr...

STM32F4 ADC DMA Transfer Error

Posted on February 06, 2016 at 18:06 I am using STM32F407VGT-6 chips. I use the DMA2 Stream0 with the ADC1 to read analog values. On two of my Boards, the code is working fine and I am not having any problems. On a third Board I programm...

Schematics for SPDIF out circuit after STM32F7

Posted on June 24, 2016 at 09:24Hello, I'm looking for information about the circuits to add to a STM32F7 Nucleo board to build an operational SPDIF output. I tried to find the information in the STM32 reference document, but could not find the inf...

jmf1 by Senior
  • 1769 Views
  • 4 replies
  • 0 kudos

STM32F4 TIM1 DMA CCR1

Posted on June 30, 2016 at 21:57I plan to use the STM32F40x TIM1 CH1 (PA8) to produce a varying  PWM  signal. The base frequency is set, say 1 MHz.  I need to use DMA to change the PWM duty cycle on every iteration. I know this can be done by aiming...