STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F427ZGT6 - Code Assisttance

Posted on July 02, 2016 at 00:51Hi, I received a cicuit board with the STM32F427ZGT6 uC on it.  I don't write code and asking for some help.  I have a push-button on PG8 (normally open) and when pressed I'd like to set PB7 high. When the push-button...

BC1999 by Associate II
  • 951 Views
  • 1 replies
  • 0 kudos

Driving TFT-LCD on STM32Fx with HAL

Posted on July 01, 2016 at 17:07 Hello guys, I am using Keil Uvision 5.2 and cube Mx for developing STM32 MCUs. and I want to Drive a TFT-LCD which the size is 2.8 inch and it has 320*240 pixels and it has ILI9328 driver inside. I have few inform...

ehsan2754 by Associate II
  • 1032 Views
  • 1 replies
  • 0 kudos

HAL Timer Triggered SPI Transfer

Posted on June 27, 2016 at 17:02 I am trying to transfer data to spi using timer 3 as a time base. Timer 3 works fine. Than I am using : DMA1 Stream2 Channel5 to trigger memory to SPI2->DR transfers, with no joy. //TIMER 3 CHAN...

ferrario by Associate III
  • 1438 Views
  • 3 replies
  • 0 kudos

STM32F4 DMA and Varying Duty Cycle

Posted on June 28, 2016 at 03:09 Hi everyone, I am wondering how to go about setting up a varying duty cycle on an F4 board using the DMA. This is for a personal project of mine, I have asked around and believe my code does not have any g...

Need help to get started with bootloader program

Posted on June 29, 2016 at 19:11I've read a few documentations from STMicro but still not sure what the actual steps to do a proper bootloading.  Here is what I understand so far.1. First the bootloader firmware is already on the uC so I don't have ...

Vu.Andy by Associate III
  • 2430 Views
  • 5 replies
  • 0 kudos

Question on USART interrupt and when it occurs

Posted on July 01, 2016 at 20:26For example, if I call the function HAL_UART_Receive_IT() with a buffer size of 16. When will the interrupt be triggered? Is it when all 16 bytes are filled up?  Or when the Usart finished received all the data? Will ...

Vu.Andy by Associate III
  • 980 Views
  • 1 replies
  • 0 kudos

Internal Clocking and Sample Rate on STM32F4 ADC

Posted on July 01, 2016 at 18:59Hi, I was wondering how the built in ADC on the STM32F4 was clocked, and how I could go about checking it's clock frequency. I know that the sample rate is configured by dividing the clock (e.g. ADC_SampleTime_480Cyc...

epalaima by Associate II
  • 1152 Views
  • 1 replies
  • 0 kudos

Problem with STM32F446FE and STM32 MAT/TARGET

Posted on June 24, 2016 at 13:26Hello everyone, I am trying to program the Nucle STM32F446FE using the STM32 MAT/TARGET and a Simulink Model, but when I build it, Simulink doen't continue with the process, blocking itself. I have downloaded the late...

julio by Associate II
  • 2036 Views
  • 4 replies
  • 0 kudos