User Activity

Posted on January 29, 2016 at 12:30 Hey guys, currently I'm working on a 4in 4out Audio-DSP based von STM32F407VGT6 with two SGTL5000 Audio Codecs. The I2S3 is the Master I2S and also generates the MCLK, I2S2 is the slave. SCLK und ...
Posted on January 21, 2016 at 23:27 Hey guys, I'm planning to make a 4 in 4 out audio dsp with f407vgt6 and two sgtl5000 codecs One i2s is master, the other is slave. They're both used in bidirectional mode. Dataformat is 24 bit lef...