STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103TBU6 forgot port pins! restore comms?

Posted on September 03, 2016 at 15:34During my first foray into CubeMX I was distracted with clock settings and forgot to configure SWDIO/SWCLK and UART pins! After flashing, STLink can no longer connect. Is there a way to rescue the chip? 

MT9M001 Camera and DCMI

Posted on September 01, 2016 at 02:08  The original post was too long to process during our migration. Please click on the attachment to read the original post.

simfake by Associate II
  • 1869 Views
  • 3 replies
  • 0 kudos

RECIVE MESSAGE IN FIFO1 ON CAN BUS

Posted on August 30, 2016 at 16:45hi evry onei working on CAN protocol with stm32f103rbt6.it working so good.now problem is here: when i reading mailboxs of FIFO0 ،all think is ok but i can not receive the message from FIFO1.please tell me how to do...

l90mehdi by Associate II
  • 3788 Views
  • 11 replies
  • 0 kudos

stm32f427 flash dual bank in application programming

Posted on August 24, 2014 at 11:47Hi! I work with STM32F427 with 2 Mb flash size and want use high flash bank to load firmware image when upgrading.When I allocate firmware image in low bank (512kb) all works properly, but when i assign address to i...

abasovag by Associate II
  • 3090 Views
  • 9 replies
  • 0 kudos

Using STM32F4's DAC with DMA

Posted on September 03, 2016 at 09:02I use DAC with DMA to ouput a sine wave. The DAC is triggered from exti9. It can output a perfect sine wave now. But I want to sync the wave's zero-crossing with a pin's rising edge. So, I put the start signal in...

Wiegand Protocol + stm32f7xx

Posted on September 02, 2016 at 19:19Hey folks,I am trying to work with an RFID reader that uses wiegand protocol, but I can't seem to find a library or any information that could help me get started. I am using a Nucleo-F767Zi board.I have found, h...

X Nucleo IDW01M1 + Custom Board + Nucleo F767Zi

Posted on September 01, 2016 at 22:48Hi folks, I am currently developing a custom expansion board for the F767Zi kit and I plan on using it along with an IDW01M1 board, the problem is I am having trouble finding out which pins from my F767Zi will be...

16- vs 32-bit CAN filter efficiency

Posted on September 01, 2016 at 18:24Is there a benefit to using 16-bit filters versus 32-bit filters in terms of MCU efficiency?  I am writing a driver for DeviceNet CAN, and the only frames I expect have standard (11-bit) identifiers, not extended...

UART IN STM32F4-DISCOVERY BOARD

Posted on August 26, 2016 at 14:48I am trying to send data (a string ''hello'') serially to my PC from STM32f4Discovery board and HC-05 (bluetooth module) using UART. I generated the following code using the STM32cubemx software. The code was succes...

13bec078 by Associate
  • 1227 Views
  • 3 replies
  • 0 kudos