STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 with LVDS Interface-LCD

Posted on September 02, 2016 at 06:59Hello everyone..I want to interface LCD which supports LVDS with STM32F429BIT6.. But I don't know what to do??I have tried many times but I couldn't get any response..It would be great for me if some one help me....

haresh by Associate
  • 1511 Views
  • 2 replies
  • 0 kudos

STM32f303 option bytes

Posted on July 06, 2016 at 00:47Hello,I am trying to read the data0/data1 fields from the flash option byte register.When the flash read protection level is 0 - I can do that no problem, but when the read protection is set to 1 it fails.According to...

USART6 RXNE?

Posted on September 01, 2016 at 15:55 I'm trying to implement an asynchronous USART using ISR to communicate with FTDI and Bluetooth Modules (RX and TX at 115kbps). I have a STM32F446RE with the following test code: void USART6_IRQHan...

New to STM32's and MCU's in General

Posted on August 26, 2016 at 10:06Hi All,My name is Dylan and I am new to STM32 MCU's and the more nitty gritty of MCU's in general. I have wet my appetite with Arduino and have had a lot of fun doing so. But I want more and so I have invested in a ...

dylan by Associate III
  • 2416 Views
  • 7 replies
  • 0 kudos

Limitations with differential ADC on STM32F3 family

Posted on September 02, 2016 at 10:18I'd like to create a multi cell Li-Ion (LiFePo4) battery monitor to measure the voltage of individual cells connected in series.  I was quite happy to find that the STM32F3 family has differential ADC capabilitie...

element by Associate II
  • 869 Views
  • 0 replies
  • 0 kudos

message transmission using GSM and stm32f303

Posted on September 02, 2016 at 09:10Hello,I am using gsm module to transmit a message using USART of stm32f303. I have used following commands for gsmAT+CMGF=1AT+CMGS=''+923046761738''at the end it requires CTRL+Z to send the message but usart is n...

STM32F407VG_Discovery IAR printf() console

Posted on September 02, 2016 at 00:16Hey Guys, i'm using the printf() to console to debug basic issues as i'm integrating an STM32F407VG_Discovery with an X-NUCLEO-IHMO2A1. In the dspin libraries to set the clocks for communicating with the L6470 Mo...

How to use the DWT_CYCCNT and DWT_CONTROL

Posted on September 01, 2016 at 19:53I am going to try some timings. I found some examples. In one example there was an address given for both registers. Is it always the same for all CPUs and is it necessary. The rest SW is with Cube. Very long lin...

LMI2 by Lead
  • 1842 Views
  • 3 replies
  • 0 kudos

Interrupt Doesn't occur

Posted on September 01, 2016 at 21:47I am working on STM32F030 Discovery. I trying to generate 1ms interrupt. But the code doesn't work. But when change the htim3.Init.Period from 0 to 1, it works with 2ms interrupt. But I need 1ms interrupt. Freque...

anuj by Associate II
  • 665 Views
  • 1 replies
  • 0 kudos