STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0 has error with Independent Watchdog Timer

Posted on October 23, 2016 at 19:03 Hi everybody! I am using STM32F030 microcontroller and I met a problem with IWDG. 1. The following code is InitIWDG() __HAL_RCC_LSI_ENABLE(); /*##-3- Configure the IWDG peripheral ################...

robotden by Associate
  • 1120 Views
  • 1 replies
  • 0 kudos

STM32F4 programming

Posted on October 22, 2016 at 15:17Hello, I'm trying to program STM32F407vgt6 chip using IAR and the code works fine but when I disconnect the power and connect it again the chip doesn't work like if the code in the flash memory was deleted and it n...

UDP connection between STM32 and MATLAB

Posted on July 31, 2016 at 22:42Hello everyone, I am using stm32f746 discovery board and I am sending 10 bytes of data in UDP protocol to PC. I can trace the data coming through LAN using WireShark application. for example No.   Time           Sourc...

abbas by Associate II
  • 1325 Views
  • 1 replies
  • 0 kudos

SD_Card

Posted on October 23, 2016 at 07:56Hi All,1. I'm writing code for the STM32F042 chip with it's evk i.e. STM32F042K6_NUCLEO.2. I'm using the IAR program to write it's code, using the supplied example named: SPI_FullDuplex_ComIT. to write into a SD_Ca...

shimon by Associate
  • 766 Views
  • 0 replies
  • 0 kudos

I have errors when debug and download code

Posted on October 22, 2016 at 14:58Error[Li005]: no definition for ''USB_Init'' [referenced from C:\Users\success\Desktop\Programme PFE ACCE_GYRO_USB\first _example\Debug\Obj\main.o] Error[Li005]: no definition for ''UserToPMABufferCopy'' [reference...

Interface two STM32F uC via FMSC

Posted on October 21, 2016 at 04:34Is possible to interface two STM32's one F7 and one F4 via the Flexible Memory Controller?Thanks for the help. #stm32f4 #fmc #fmsc

mazielvc by Associate II
  • 1959 Views
  • 3 replies
  • 1 kudos

STM32F746, Pixel erros with VRAM in remapped SDRAM

Posted on October 22, 2016 at 22:41Hi there,I have a F7 setup with running LTDC, DMA2D and SDRAM to drive a tft display. The VRAM buffer is defined in SDRAM memory.When I use the standard SDRAM address mapping at 0xC0000000, the display works fine w...

Hard Fault with USART & Ethernet

Posted on October 22, 2016 at 09:08The original post was too long to process during our migration. Please click on the attachment to read the original post.

parisa by Senior
  • 1600 Views
  • 2 replies
  • 0 kudos

DFUSE Demo bricks STM32L476

Posted on October 21, 2016 at 21:00 We had success updating our device with the DFUSE demo which uses a STM32F4 device. We now have a product with a STM32L476 device, but when I try to update it via DFUSE demo, it bricks it. To get the de...

seb2 by Associate
  • 1314 Views
  • 2 replies
  • 0 kudos