cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 DSP and standard peripherals library - bug in I2C_CheckEvent() ?

Andrew Neil
Super User
Posted on May 07, 2016 at 16:00

Reference manual RM0383, ''STM32F411xC/E advanced ARM®-based 32-bit MCUs'', says:

6.7 I2C Status register 2 (I2C_SR2) Note: Reading I2C_SR2 after reading I2C_SR1 clears the ADDR flag, even if the ADDR flag wasset after reading I2C_SR1. Consequently, I2C_SR2 must be read only when ADDR is foundset in I2C_SR1 or when the STOPF bit is cleared. But theSTM32F4 DSP and standard peripherals library, STSW-STM32065, does not do this in I2C_CheckEvent():

ErrorStatus I2C_CheckEvent(I2C_TypeDef* I2Cx, uint32_t I2C_EVENT)
{
uint32_t lastevent = 0;
uint32_t flag1 = 0, flag2 = 0;
ErrorStatus status = ERROR;
/* Check the parameters */
assert_param(IS_I2C_ALL_PERIPH(I2Cx));
assert_param(IS_I2C_EVENT(I2C_EVENT));
/* Read the I2Cx status register */
flag1 = I2Cx->SR1;
flag2 = I2Cx->SR2;
flag2 = flag2 << 16;

It will always read SR2 immediately after SR1 - without any attempt to check ADDR or STOPF. I guess it should look something like this:

/* Read the I2Cx status registers */
flag1 = I2Cx->SR1;
/*
* RM0383 states, ''I2C_SR2 must be read only when ADDR is found
* set in I2C_SR1 or when the STOPF bit is cleared''
* See section 6.7 I2C Status register 2 (I2C_SR2) on page 492 (Rev 1).
*/
if( (flag1 & I2C_SR1_ADDR) ||
(flag1 & ~I2C_SR1_STOPF) )
{
flag2 = I2Cx->SR2;
}
else
{
return ERROR;
}

(can't raise a ticket on this as the system is down for ''upgrades''). This is in the current 1.7.0 library release, and previous releases. #library #stm32f4 #i2c
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Nesrine M_O
Lead II
Posted on May 23, 2016 at 18:42

Hi neil.andrew,

Thank you for your feedback. The issue has been reported internally.

-Syrine-
Posted on May 23, 2016 at 21:32

Download page says F4 DSP 1.7.1 but is actually 1.7.0 per directory

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-standard-peripheral-libraries/stsw-stm32065.html

Can we get an update of the forum post linking to all old firmware releases, please.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..