STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is this possible with complementary PWM?

Posted on December 22, 2016 at 12:43 Hello everyone, I want to ask something about Advanced Control Timers. In RM0008, I saw an example (Fig. 95) but I can't understand how it is possible. I tried an example and my PWM signals (ex. on Fig. 95...

Cemre . by Associate II
  • 2120 Views
  • 4 replies
  • 0 kudos

Interupt responstime issue stm32f429 vs stm32f767

Posted on December 14, 2016 at 14:36hello,I'am use for a project the stm32f429. The interrupt handler must react so soon as possible.The stm32f429 interrupt responstime is 218ns.It's  fast but not fast enough. I decided to make a new design with the...

Hans T by Senior
  • 5091 Views
  • 15 replies
  • 0 kudos

STM32F4 TIM1 One Shot Mode configuration

Posted on November 29, 2016 at 23:27Greetings,I am trying to achieve the following with TIM1 and TIM1_CH1:1. Generate X number of PWM pulses after an event.2. Idle state of PWM output should be low.3. Pulse output should be high immediately after PW...

rcstang by Associate
  • 2986 Views
  • 3 replies
  • 0 kudos

Touchscreen linearity on STM32F469 issue

Posted on December 11, 2016 at 01:29After spending a lot of time with an STM32F469 discovery board I found that the touch screen doesn't have good linearity at all.  You can't draw a straight line across the screen.  If you for instance, start on th...

STM32F407G-DISC1 - cannot access memory

Posted on December 22, 2016 at 15:02Hi,after working with this board fine for a while I now have a problem. Using Keil when I tried to LOAD the program a message reads: 'Flash Timeout. Reset the Target and try again.'. I tried a lot of things, from ...

How to control CS independently of SRAM R/W ?

Posted on December 21, 2016 at 20:37Hello,We use LCD interface with SM32F4 , with ILITEK 9341.According to LCD datasheet is it required that CS will be kept active throught several writings of data/control.But We see that each write of 8-bit word re...

ranran by Senior II
  • 1682 Views
  • 3 replies
  • 0 kudos

How to clear HAL_BUSY situation for I2C

Posted on December 22, 2016 at 14:36Hello,On my board I have 2 STM32 processors which communicate to each other over I2C. One is always a master and the other one is slave.The slave prepares some data, and then I do:   HAL_I2C_Slave_Receive_ITand wa...

srdjan by Associate II
  • 2031 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F4 TIM6 interruption doesn't happen while DMA working

Posted on December 22, 2016 at 10:14 I work with STM32F4Discovery board, generate code from Cube, SYSCLK is 168MHz, APB1 Timer Clock 42 MHz, TIM6 has prescaler 1000, and counts till I make the following experiment. Enable TIM6 interruption by...

kozlovdmn by Associate II
  • 2769 Views
  • 4 replies
  • 0 kudos