Skip to main content
Barbie
Associate III
August 4, 2016
Question

ADSTP not work on STM32F030R8T6

  • August 4, 2016
  • 0 replies
  • 570 views
Posted on August 04, 2016 at 09:35

Some time on my run I see that even if I do ADC1->CR |= ADC_CR_ADSTP;

And wait on  while ((ADC1->CR & ADC_CR_ADSTP) != 0);

It didn't go to ''0''.

I check and see that ADSTART=''1'' and ADDIS=''0''.

It configure to ADC1->CFGR1.EXTEN =0x01 and ADC1->CFGR1.EXTSEL=0x04. Also ADC1->CFGR1.DMAEN=1.

As I understand the ADSTP make the ADC stop any conversion , But if it is wait for converstion by ext trigger which won't come (if the timer was disable before), does this bit will stay ''1'' for ever?

If so,what should I do to be sure it is in a middle of conversion?

Regards

Bar.

#adstp-stm32f030r8t6
This topic has been closed for replies.