STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F3 EEPROM Emulation -> HardFault

Posted on February 06, 2017 at 16:06Hello,i try to implement the EEPROM Emulation for the F3 to my Motor Control Application.But inEE_Init()afterPageStatus0 = (*(__IO uint16_t*)PAGE0_BASE_ADDRESS);i get a Hardwarefault.I added the Files eeprom.c and...

s61331 by Associate II
  • 2572 Views
  • 5 replies
  • 0 kudos

Knx C library

Posted on February 07, 2017 at 14:43Hello, I am interested KNX protocol  with STM32F7 series processors  nowadays, I want to make some applications with KNX protocol. But I didn't find free KNX Stack for C library. Where can I find to use this free ...

ali2399 by Associate II
  • 2347 Views
  • 2 replies
  • 0 kudos

STM32L4 UART+DMA

Posted on January 10, 2017 at 20:37I have an RTOS app running with few tasks though I don't think it matters if you use OS or not anyway. Basically every now and then I get random errors like FE (framing error), ORE (overrun error), NF (noise flag s...

ChrisH by Associate III
  • 5568 Views
  • 10 replies
  • 0 kudos

Question on ADC with DMA circular mode

Posted on February 06, 2017 at 19:12Hi everyone,I'm a newbie and I'm working on ADC with DMA in circular mode like pictures below:and a part of my code is:HAL_ADC_Start_DMA(&hadc1,(uint32_t*)buffer,sizeof(buffer));while(1){for(i=0;i<=255;i){}}When I...

0690X00000606FvQAI.png 0690X00000606FzQAI.png

Can STM32F103RB6 operate via I2C with STM8S103?

Posted on February 07, 2017 at 16:57I want to use STM32F103RB6 MCU to connect to STM8S103 MCU via I2C. Can I get data of STM8S103 via STM32F103RB6 and control the operation of STM8S103 by STM32F103RB6 via I2C interface? These two MCUs operate in dif...

hkwong by Associate
  • 1338 Views
  • 2 replies
  • 0 kudos

Resolved! SPI BSY erratum listed under I2C in 'F76x/77x errata

Posted on February 07, 2017 at 14:29In STM32F76xxx and STM32F77xxx silicon limitations DocID028806 Rev 4, 2.2.2  BSY bit may stay high at the end of a data transfer in slave mode which is entirely an SPI error, is listed under I2C peripheral limitat...

I2S swapped L/R channels after I2SResume

Posted on February 06, 2017 at 23:24Hello,I collect the ADC data through the I2S1 peripheral using DMA2Once1) i collected certain amount of results,2) the reception is paused with:HAL_I2S_DMAPause(&hi2s1);3) I send the data through UART4) then the r...

akosodry by Associate II
  • 4116 Views
  • 5 replies
  • 0 kudos