STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F030K6T6 usart library?

Posted on March 08, 2017 at 11:36hifirst i look herebut there is no usart driver.this is my schematicaccording to schematic i use pa2 and pa3 as usart.please tell me if there is any library to init usart and use it.if there is not .datasheet give me...

0690X00000606VOQAY.png 0690X00000606VxQAI.png

INTEST:JTAG Boundary Scan

Posted on February 01, 2017 at 13:16Hello Everyone,I have built a pcb consisting stm32L152V8t6 and other peripherals.I am trying to use JTAG Boundary Scan to test the functionality of the chip. So currently I used the TopJtag(http://www.topjtag.com/...

dhiraj by Associate II
  • 5652 Views
  • 6 replies
  • 0 kudos

OsxAcosticBF R/L data sequence

Posted on March 08, 2017 at 05:39Hi all,I am struggling to  know L/R data sequence in OsxAcousticBF project which provide by St-microelectronics.can you please help me to find out what is data sequence of OsxAcousticBF project.i dump data like that ...

STM32F072 CAN Interrupt as Stop Mode wakup

Posted on March 07, 2017 at 17:03Hello,In my project I need to run Stop Mode on STM32F072, but also I would like to monitor CAN Bus and wake it up when some specific ID will be send. Is it possible ? I'm trying and it's not working ?I did set up CAN...

Using STM32F446xx TIM2, how to measure frequency > 1Mhz.

Posted on March 06, 2017 at 23:45Hello All, I am using STM32F446xx TIM2 to measure frequency > 1Mhz. I have set TIM2 to external clock and see the counter increment at every rising edge. I am reading this counter value in main function for test. But...

Resolved! STM32F207 Uni Directional SPI - Rx using DMA

Posted on March 07, 2017 at 01:30Hi Everyone,my set-up is an STM32F205 transmitting fixed length data ( < 64 bytes ) periodically to an STM32F207 via SPI. I am only interested in receiving data, nothing is sent on the 207's MISO line.The 207 receive...

Resolved! SPI3 in stm32f10x problem

Posted on March 02, 2017 at 08:53Hi,Sorry I take the forum user's time for my simple questions.Here is my code for spi3 in stm32f10x for PB3 and PB4 output/input.    SPI_InitTypeDef SPI_INS;      GPIO_InitTypeDef GPIOS    RCC_APB2PeriphClockCmd(RCC_...

0690X00000606SeQAI.png
parisa by Senior
  • 930 Views
  • 1 replies
  • 0 kudos

Can someone suggest a gand programmer for stm32L152V8T6A?

Posted on March 07, 2017 at 14:39Hello ST_Community,       I am using the stm32L152V8T6A in my device and soon want to make its multiple copies.So can someone suggest the best suitable gang programmer to flash the firmware in multiple devices?.I am ...

dhiraj by Associate II
  • 850 Views
  • 1 replies
  • 0 kudos