cancel
Showing results for 
Search instead for 
Did you mean: 

Jumping to flash address in other bank

ghislaindavost
Associate
Posted on October 12, 2016 at 15:07

Hi!

I work on a Nucelo 144, with STM32F4 I try to make a jump starting from the start application (sector 1, address 0x8000000, bank 1) to another application contained in Sector 17 ( address 0x8120000, bank 2). I made a code by helping me an example of IAP with jump_to_app function. The jump is not working. The problem might be for the management of the vector table ? main.c

#define SECTOR_5_ADDRESS 0x08020000 //PROG #2
#define SECTOR_17_ADDRESS 0x08120000 //PROG #1
/* Jump_Sector17 Parameters */
typedef
void
(*pFunction)(
void
);
pFunction Jump_to_application;
uint32_t Jump_address;
void
Jump_Sector17(
void
);
int
main(
void
)
{
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize GPIO peripherals */
MX_GPIO_Init();
HAL_GPIO_WritePin(GPIOB, LD2_Pin, GPIO_PIN_SET);
Jump_Sector17();
#endif
}
void
Jump_Sector17(
void
)
{
/* Set system control register SCR->VTOR */
NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x12000);
/* Jump to user app */
Jump_address = (*(__IO uint32_t*) (SECTOR_17_ADDRESS + 4));
Jump_to_application = (pFunction) Jump_address;
/* Initialize to user application */
__set_MSP(*(__IO uint32_t*) SECTOR_17_ADDRESS);
Jump_to_application();
}

system_stm32f4xx.c

#define BL
/* #define VECT_TAB_SRAM */
#ifdef BL
#define VECT_TAB_OFFSET 0x12000 /*!< Vector Table base offset app. */
#else
#define VECT_TAB_OFFSET 0x00 /*!< Vector Table base offset boot. */
#endif
/* This value must be a multiple of 0x */

I hope that my explanation was clear, english is not my native language. Thank you in advance for your help.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on October 12, 2016 at 19:49

The problem might be for the management of the vector table ?

Or what is in the Vector Table. Make sure you built it for the address you have placed it.

Consider using a debugger and stepping across the transition and into the startup code on the other side. Perhaps you can refine ''not working'' into something more specific about what IS happening.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..