Question
Which USB device class to choose?
Posted on October 12, 2016 at 22:27
Hey guys
i'd like to use my STM32F4 to transfer data from the MCU to the PC (and vice versa). I thought it would be the easiest for the PC to be the host and the MCU to be the device, therefore i have worked my way through theSTM32Cube USB device library.
Now if i got this correct there are 3 possible fitting classes HID Class pro: does not require an extra (Win) PC driver, which is pretty nice cons: only 64 byte per packet (i'm not so sure if this limit only applied to the config channel or all channels, maybe you can enlighten me ;)) CDC class: pro: seams to be easy to use cons: does need an extra VCP driver (on windows) last but not least: the mass storage class pros: seems to be ideal for very large data ?! cons: does it require an extra driver? could you fill in my blanks? Which of these classes would you use?