STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Calculate rcc with stm32f10x

Posted on March 14, 2017 at 17:23Hi,Here is my input datayou assume that I have 4 variables such as Data1,Data2,Data3 and Data4 that store each byte (Data1 saves d24-d31 and Data4 stores D0-D7). So I want to know how can I execute Crc-8 algorithm in...

0690X00000606F3QAI.png
parisa by Senior
  • 2408 Views
  • 9 replies
  • 0 kudos

''ARM compiler for MCU'' ver. 1.13.2 Error in System Workbench

Posted on March 18, 2017 at 10:48Hi,Recently I upgrade the 'ARM compiler for MCU' in System Workbench to 1.13.2 after which I am getting the following error as displayed in the console :/usr/make/sh: arm-none-eabi-gcc: command not foundmake: *** [Da...

RADS1 by Associate II
  • 693 Views
  • 0 replies
  • 0 kudos

STM32L053 EEPROM writing going to HardFault

Posted on March 17, 2017 at 23:00Hi!I am trying to write s string into the EEPROM of a STM32L053.I create a strcpy like funtion, using STM32L0xx HAL Libraries:for writing the EEPROM I use this sequence of HAL functions.char ascii_string[200];HAL_FLA...

CAN Initialization on extremely high traffic

Posted on March 17, 2017 at 21:30Hi, my software stucks on CAN_MSR_INAK acknowledge when I try to init CAN in device that is connected to network with very high traffic. From reference manual I've found that:  Once 11 consecutive recessive bits have...

SMTF32F1x CAN bus Error Frame

Posted on February 17, 2017 at 18:54Hi,I am seeing Error Frame from one of our project using STM32F1x MCU. Any recommendation how to debug this issue?Thanks,Dick112.227000 1 108 Rx d 8 db 1f c0 69 ee 89 e8 3e 112.227000 1 109 Rx d 8 86 31 94 43 00 ...

Custom external bootloader on custom F769I based Board

Posted on March 16, 2017 at 18:29Hi community,I need to write an external bootloader for my custom board based on the stm32f769I MCU.According to the 'STM32 ST-LINK utility software description' manual, I have to modify one of the exemple provided a...

enia ami by Associate II
  • 2766 Views
  • 6 replies
  • 0 kudos

Audio_Sampling_frequency

Posted on March 17, 2017 at 10:30Hi all,I am working on memsmic1 application which is convert 1 bit pdm data into pcm. with sampling frequency 16 Khzif#define AUDIO_CHANNELS 2#define AUDIO_SAMPLING_FREQUENCY 16000 #if (AUDIO_SAMPLING_FREQUENCY == 16...

How to revive a dead MCU in-circuit?

Posted on December 18, 2016 at 15:11Hello all!  How's this for my very first question I purchased a 3d Printer on clearance with a tag that says Does not Start up.  No warranty.  I was ok with that.  As I'm a developer and a hardware hacker I knew I...

Resolved! STM32F437 timer input capture

Posted on March 16, 2017 at 20:16I have attempted to set up timer 4 channel 1 for input capture but unsuccessfully. The scope indicates that my 1KHz, 3vdc, 35 uSec pulses are making it to PD12 (TIM4, ch 1). However, CC1IF is never set. Although chan...

John Hite by Associate III
  • 1779 Views
  • 5 replies
  • 0 kudos