STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 ILI9341 non-arduino example request

Posted on April 23, 2017 at 02:47Hello!I want to control ILI9341(SPI LCD) by STM32F103C8.Simple SPI access is ok.Most example are belong arduino in internet, but I am using EWARM.Please share your experience to me.BRLC

L C by Associate II
  • 1954 Views
  • 4 replies
  • 0 kudos

STM32F042 Encoder Problem

Posted on April 28, 2017 at 20:24I'm using the stm32f042 nucleo board, Atollic truestudio and CubeMX launched from the Atollic GUI (eclipse) to develop code. I am trying to get the encoder interface on timer 3 to function as a step/dir counter. I ha...

Resolved! STM32 CubeMX Installation Problems Mac

Posted on April 27, 2017 at 14:46Hi everyone,I turn to you in complete despair. I thought I would start tonight with My Nucleo, but couldn't even get past the Installation of the CubeMX software. When I double click on the app (SetupSTM32CubeMX-4.20...

stm32f103 button interrupt not working

Posted on March 23, 2017 at 09:22Hi All,I am working on button press interrupt on stm32f103 . I am not able to get it into work. I am not at all receiving any interrupt when the button which is connected to PORT B 12 13 14 is pressedBelow is my code...

Don david by Associate II
  • 2197 Views
  • 3 replies
  • 0 kudos

SD MMC Power on issue (STM32L4)

Posted on December 15, 2016 at 08:55 Hi, I'm developing a firmware for a custom board with a STM32L486 microcontroller. The device record the audio to a micro SD card. I'm using the HAL driver. It's work fine with at least 6 ...

Null modem with full handshaking for STM32F3DISCOVERY

Posted on April 28, 2017 at 12:03Hi,I would like to control the E3631A power supply by RS232.I use the null modem without handshaking (RX, TX and GND).I can set the power supply but when I use *IDN? or SYSTem:ERRor? command.The power supply didn't r...

Good B by Associate II
  • 988 Views
  • 3 replies
  • 0 kudos

SW4STM32 + STM32F411E Disco

Posted on March 21, 2017 at 12:47When I try to run and debug a project with SW4STM32-Eclipse I get the following error message:Error in final launch sequenceFailed to execute MI command:-exec-runError message from debugger back end:Don't know how to...

Luca R by Associate II
  • 864 Views
  • 3 replies
  • 0 kudos

STM32F030: Interrupt remaping to RAM

Posted on April 28, 2017 at 04:33Hi,I am developing bootloader for STM32F030ccT6 to upgrade my Main Application through OTA. There are two application within my controller flash one is BOOTLOADER( @ 0x08000000) and other is Main Application( @ 0x080...

STM32F103 SPI question

Posted on April 28, 2017 at 12:57This is the first time I need SPI, and there are two things that are still unclear to me:1) I understand that to receive from a slave, I need to send something - maybe zeros?So if I have a chip that takes register ad...