STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reading incoming PWM signal

Posted on May 14, 2017 at 03:23How can i read an incoming PWM singal coming from my rc receiver ?? i kept searching and i found something called input capture but i couldn't understand it ?? so i will be glad if you can provide me an example.

Resolved! Nucleo STM32F103RB : cannot blink a led on GPIO B3

Posted on May 15, 2017 at 20:37Hi everybody,I can't blink a led on GPIO B3 (PB3) port , the code works well on another ports like PB5 PA5... but not on PB3.I have buy another nucleo board cause I was thinking I have an issue with my previous board b...

eLuigi by Associate II
  • 3041 Views
  • 6 replies
  • 0 kudos

issues of virtual communication of Nucleo board

Posted on May 16, 2017 at 11:16Hello everyone:i met a big problem, now i am using Nucleo L073RZ board and x-nucleo-ids01a5 expansion board to do the point to point communication. i want to use SPIRIT1 DK to receive and analyse the data. however, i c...

0690X00000606xYQAQ.png 0690X00000606z0QAA.png

Programming STM32F051K8

Posted on May 17, 2017 at 07:46Hi,I am working on STM32F072CB for my custom board, for programming this, I am using NUCLEO-70RB board.I have a separate board having STM32F051K8T6 mcu. I just want to know, can I program STM32F051K8T6 with NUCLEO-70RB...

akshat by Associate II
  • 610 Views
  • 0 replies
  • 0 kudos

ADC voltage reference selection (F7).

Posted on May 16, 2017 at 18:50Coming form AVR to STM32 F7 46, can I select voltage reference for ADC. Like in AVR, I could choose AVDD or VREF. Besides, If I connect 2.5V to the VREF and 3.3 to AVDD, then what is the range of ADC measurement?1) Is ...

zupazt3 by Associate
  • 1173 Views
  • 1 replies
  • 0 kudos

[C++ STL] Pretty Printing?

Posted on May 17, 2017 at 01:16Hello C++ afficionados,has anybody successfully worked out how to use gdb pretty printing for displaying the contents of stl containers here?Especially for Atollic TrueStudio?If so, could somebody give me a hint on how...

Error in compiling 746 Discovery demo

Posted on May 16, 2017 at 19:47I am studying the STM32F746 Discovery board and tried to compile the demoC:\Users\LM7\STM32Cube\Repository\STM32Cube_FW_F7_V1.7.0\Projects\STM32746G-Discovery\DemonstrationI am using Keil 5.*** IDE.It gave me an error:...

LMI2 by Lead
  • 3062 Views
  • 3 replies
  • 0 kudos

STM32 HID Multiple Endpoint

Posted on May 14, 2017 at 02:40Hi I would like to ask if it is possible to use 2 end point for HID device?for example: EP1 IN and out for maintenance commands/statusthen EP2 IN and out for remote command and statusfor transfer mode, i like to have t...