STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ISSUE with Erase Command of STM32F4 CAN Bool loader

Posted on June 20, 2017 at 22:02I'm using the CAN Boot loader on the STM32F405xx chip and have an issue with the Erase command (0x43).I am able to execute 0x00, 0x01, 0x02, 0x11, 0x21 & 0x31 as described in the Protocol Document, however when ID: 0x...

SD Card interface with STM32F303

Posted on September 06, 2016 at 08:13Hello,I want to interface a SD card with stm32f303. Please help me how to interface sd card with microcontroller. Also I want to read the data on my laptop, do I need a file system because windows can read in FAT...

2013ee139 by Associate II
  • 1875 Views
  • 3 replies
  • 0 kudos

STM32F334, DAC Out and Comparator

Posted on June 24, 2017 at 21:14Hi,Looking at STM32F3348-Discovery_FW_V1.0.0\Projects\Demonstration\main.cand AN4885 (en.DM00115322.pdf)Looking at overcurrent protection with COMP4(+)(PB.0) connected to Current SenseI am wondering whether the DAC Ou...

Duplicated OUT report in HID

Posted on June 24, 2017 at 19:12I am developing HID application on STM32F427 with STM32_USB-Host-Device_Lib_V2.2.0Works mostly fine, but once in a while (quite often, actually), when Windows app sends command to the controller (OUT report), it's dup...

Ethernet reception - STM32F437

Posted on June 23, 2017 at 23:37We used to have a simple PHY attached to the MII port and it seems the less you did to configure it the better. Now we have replaced it with a Marvell 10 port switch. Two of the ports have no phy and are setup to talk...

John Hite by Associate III
  • 792 Views
  • 0 replies
  • 0 kudos

STM32L471 WFI problem

Posted on June 20, 2017 at 17:43On STM32L471 (DEV_ID=0x6415, REV_ID=0x1007)~4% of mcus do not enter standbymode and ignore the WFI instruction.Does anyone have ideas how to get it working on all mcus? (tested with 150 pieces)Is there any known bug/p...

damh by Associate II
  • 1698 Views
  • 3 replies
  • 0 kudos

Backup SRAM write failure (STM32F446)

Posted on June 22, 2017 at 07:20Hello.I have an issue using the backup SRAM on a STM32F446.The backup SRAM is used to store calibration data  which must be retained in case of a power fail reset. For that I connected the VBAT pin to a capacitor whic...