cancel
Showing results for 
Search instead for 
Did you mean: 

Bug: Cube 4.17.0 and STM32Cube FW_F4 V1.13.1 ADC1 temp sensor and vref

Andrei Chichak
Lead II
Posted on October 11, 2016 at 20:54

I just updated Cube to 4.17.0 and my project now has issues with the channels being used in ADC1.

Two files attached. Screen shots. First one showing the processor temperature probe and vref channels being declared as Value not found. The second showing the item in the pick list being chosen. The problem remains after a value has been chosen from the pick list.

Yes, the temperature probe and vref are enabled in the Pinout tab.

Yes, the problem persists if I choose a different channel, save, choose temperature, save.

Yes, the problem persists if I turn it off and back on again.

BTW, thank you (not) for renaming mxconstants.h to main.h in the Inc directory. My tutorial, that I posted just this morning, is now broken.

Andrei

embedded.fm/blog

 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen.D
ST Employee
Posted on October 21, 2016 at 17:20

Dear User,

Please note that your feedback is reported to our STM32CubeMX team and it is under review.

Best Regards

STM32.forum

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Jeanne Joly
Senior III
Posted on January 09, 2017 at 16:38

Hello Andrei Chichak,

Sorry for the delay. 

The issue you reported is corrected and already delivered in CubeMX4.18.

BR.

Eric Dampierre.

Posted on January 09, 2017 at 19:34

Yes, and in early October it was incorrect.

Have a better day,

Andrei from The Great White North.