STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

cube 4.21 hangs generating code

Posted on May 11, 2017 at 14:51I did upgrade to cube 4.21 and for 1 project, when generating the source code, cube MX hangs.I have to specify that it hangs only for 1 of my project.

Adalgiso by Associate II
  • 3274 Views
  • 8 replies
  • 0 kudos

STM32F051 as i2c slave - not 100% successful

Posted on July 04, 2017 at 01:17 Hi, in my implementation, i2c slave address recognition on STM32F051 is not 100%. Followingcommunication works well. I'm using DMA.When I set HCLK frequency to 8MHz (from HSI source), probability of address A...

kumen by Associate II
  • 1004 Views
  • 1 replies
  • 0 kudos

onboard st-link

Posted on July 05, 2017 at 19:52Are there no provisions to support on board ST-Link?  I would like to include ST-Link as part of my design.

CubeMx LwIP update for F1 series?

Posted on June 21, 2017 at 11:14Hello,im working with the STM3210-C Eval board (F107VC microcontroller). I recognized that for F1 series there is in CubeMx (ver.4.21.0) only a LwIp version 1.4.1 available while for F4 series there is version 2.0.0 i...

Resolved! Why do spi transfer insert delays between byte transfers

Posted on July 05, 2017 at 15:53STM32F091xc processorOne spi controllerI'm doing transfers to a LCD.  The LCD appears to somewhat work.  However the colors and orientation seems odd.  I looked at the SPI bus on Logic Analyzer and I get delays betwee...

0690X00000607I2QAI.png

STM32F1xx CAN Again

Posted on July 05, 2017 at 12:11Hi,i'm working with little project on STM32F105, but libraries have never been corrected from STM and bugs are presents also on last version* @version V1.0.4* @date 29-April-2016.Now i have a little doubts about STM l...

Marco1 by Associate II
  • 851 Views
  • 1 replies
  • 0 kudos