STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

possible bug in clock generation

Posted on June 09, 2017 at 09:26I am using cube 4.21 with a STM32F205 CPU.I configured the clock to run at 120 Mhz (25Mhz crystal M=20, N 192, P 2) in the file system_stm32f2xx.c generated by cube, I have the following:uint32_t SystemCoreClock = 160...

Adalgiso by Associate II
  • 1660 Views
  • 3 replies
  • 0 kudos

How to program ''single byte'' to STM32 internal flash?

Posted on July 06, 2017 at 04:17Hi, all!    I want to program single byte to internal flash, but the standard peripheral library only support 'word' and 'half word', is it possible to program single byte, please?For example: mailto:0x11@0x08010000, ...

Resolved! Interrupts - USART corrupted data

Posted on July 04, 2017 at 11:16Hi everyone,I am designing a system that needs a bunch of interrupts working. By now I have three possible source of interrupts working:+ USART6+ SPI2+ TIM6The USART6 works sending and receiving data from PC.When SPI2...

Build error 238 on example/user/main.o

Posted on July 05, 2017 at 15:15I have a P-NUCLEO-IHM001 board and try to build an example from the directotry 'STM32Cube_FW_F3_V1.8.0' with AC6 toolchain and always get a build error 238 on example/user/main.oWhy does this occur and how can I solve...

Improve code processing time

Posted on June 27, 2017 at 19:18 I am working with the STM32L486 and we aim to use as low clock speed as possible to conserve power. As a result, I need to improve the run time inside one high rate interrupt to meet the timing requirement. I was tr...

e d by Associate II
  • 9088 Views
  • 26 replies
  • 0 kudos

STM32F107RC bootloader and datecode

Posted on July 06, 2017 at 11:01Hello,we have a board with the STM32F107RC controller in TQFP64 package. According to the AN2606 chapter 13.3.2 the internal bootloader is not available on our package with a date code below 937. However the date code...

issue with USB ULPI

Posted on July 06, 2017 at 10:38Hi,please could anybody help me to find out what is wrong ?i made 2 boards,first one is using STM32F779 and second one STM32F756,from USB ULPI point of view they have same schematics and same PCB layout (connection to...