STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H723 Nucleo: UART4 not working

I am stumped and frustrated. I wrote some test code to test UART4. It worked fine. Then I moved the test code over to my main project and now I get no UART interrupts. Both code sets run on the same hardware. I have checked to make sure the UART RX w...

Adjusting XSPI RAM Clock at runtime

Good day folks, I trust you are well.I am interfacing with a APMemory 256Mbit RAM (APS256XXN-OBR) via the 16 way XSPI.The RAM registers can be configured correctly at 100MHz, as well as the whole 256 Mbits can be accessed via Mmap.For Configuration I...

exarian_0-1739428461225.png
exarian by Associate III
  • 1780 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G431 unable to enter bootloader mode

I have a custom PCB with the STM32G431 microcontroller and ESP32 controller. ESP32 is connected to STM via GPIO pins in order to perform firmware upgrade using STM32 bootloader protocol. Connection are as follows:ESP32 UART TX <-----> STM32 UART RX (...

Buck converter with peak current mode -Sawtooth generator

Hii, I'm new to embedded systems. I have the B-G474E-DPOW Discovery kit with STM32G474RE MCU and I implemented the peak current mode Buck converter(HW) as described in the application note of stm. The only thing that I cannot understand is how exactl...

Fani by Associate
  • 1454 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H5 Interface With Gigabit Ethernet PHY device

Moved from MPUs forum.Hi, i must Use a Single Port Gigabit Ethernet PHY  that have a RGMII Gigabit Interface to connect a RMII 10/100 MbitEthernet MAC interface of the STM32H563VI MCU. Do you think it is possible to connect a Gigabit PHY chip to the ...

B.Michele by Associate III
  • 6763 Views
  • 10 replies
  • 3 kudos

Wrong echo from STM32F4 USB device

Hi all,I'm developing a composite USB device on USB OTG port on a board based on STM32F429 chip.The device has two interfaces: a custom device + a CDC device. I'm using USB_Device_Library code.Windows host correctly shows 3 items: the composite devic...

SteMMo by Senior
  • 4911 Views
  • 7 replies
  • 1 kudos