STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with FMC_NOR Sample Program.

Posted on September 04, 2017 at 07:45I am working on STM32F756-EVAL2 Board, and wanted to use NOR Flash Memory to Store some configuration data. But i am facing some problem. I am not able to write any thing into NOR memory.(But able to perform read...

STM32L4 Standby Pulldowns on PA15

Posted on September 04, 2017 at 02:20Hi Guys,I am running a STM32L452 on a custom board using the STM32Cube HAL. I am putting the uC into standby mode and am configuring some of the pins to pull up/down using the functions in the stm32l4xx_hal_pwr_e...

Chris H_2 by Associate II
  • 2398 Views
  • 3 replies
  • 0 kudos

How to create a CMSIS project for DiscoveryF407VG board?

Posted on September 03, 2017 at 19:09I have downloaded Keil 5.24a, and Arm cortex-M legacy support, when I want to create a new project, in micro selection step, in Software Packs there is no STM32F407VG micro, but there is STM32F407VGTx micro inste...

m m by Associate II
  • 1948 Views
  • 4 replies
  • 0 kudos

STEVAL-ISV002V1 SOURCE CODE

Posted on September 03, 2017 at 19:23Hi there, I recently started a project involving application note 3095. I'd like to konw if there any way to get its source code (STEVAL-ISV002V1 STEVAL-ISV002V2 BASED STM32F103XX)?! If someone already tried or k...

Where can I get the souce code for AN3322?

Posted on September 04, 2017 at 00:54Hello, I am trying to build my own watt-hour meter for my home using an olimex e407 board. After a little bit of research I found this application note (http://www.st.com/content/ccc/resource/technical/document/a...

STM32F411: I2C_FLAG_AF set but no I2C interrupt is set

Posted on September 03, 2017 at 12:05I am designing a slave process that shall manage unpredictable write/read request from the master.Unpredictable: the slave doesn't know in advance how many bytes are going to be written from the master, and how m...

Luca R by Associate II
  • 1109 Views
  • 0 replies
  • 0 kudos

How to update the programmable alarm

Posted on August 20, 2017 at 19:15Hi every one I want update the programmable alarm in stm32f4 series .according to reference manual :Programming the alarmA similar procedure must be followed to program or update the programmable alarm (AlarmA or Al...

l90mehdi by Associate II
  • 2887 Views
  • 6 replies
  • 0 kudos

Resolved! Why AF input as push-pull?

Posted on September 02, 2017 at 20:14 What is the idea that in many cases alternate function inputs are configured as 'alternate function push-pull'? In most cases it seems to work, but why? From the documents I've got the idea that the inputs ar...