STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem in communication of STM32F429 with STMPE811

Posted on August 25, 2017 at 07:00 Hello, I used STM32F429 for communicating with STMPE811 through SPI port. In the beginning, I read chip ID of STMPE811 in order to make sure communication is correct. Sometimes, IC doesn't return anything. I...

ali by Associate II
  • 5504 Views
  • 10 replies
  • 0 kudos

Resolved! Is there SPL library of STM32F4x?

Posted on September 04, 2017 at 15:45Hi.I bought 2 eval boards STM32F429I-DISC1 and STM32F10x-DISC1 and found STM32F10x_StdPeriph_Lib_V3.5.0 of  STM32F10x.But  I'd like to get STM32F4x SPL file not en.stsw-stm32054.zip STM32F10x_StdPeriph_Lib_V3.5.0...

STM32F10x interrupt example question

Posted on September 04, 2017 at 05:42HI.Currently I'm trying to understand about STM32F10x's interrupt.So I've got some snippet code as the below,USART1's IRQ number is 37.// interrupt example snippet code //unsigned int vector_table_start_addr = *(...

0690X000006041IQAQ.jpg

STM32F0 cortex jump to application

Posted on August 31, 2017 at 16:29Hello to all, I need to write the bootloader for a cortex M0. Could someone explain to me what I have to do. What are the code that I have to write and how I have to modify the linker and the sturtup .s file? In the...

Giu S by Associate II
  • 4849 Views
  • 8 replies
  • 0 kudos

What is the value of tsu(Data_NE) + tv(A_NE) on STM32F207

Posted on September 04, 2017 at 09:49In AN2784:Using the high-density STM32F10xxx FSMC peripheral to drive external memories.There is a rule:tsu(Data_NE) + tv(A_NE)=2tHCLK + 25. I use STM32F207 on my board. What is the value of tsu(Data_NE) + tv(A_N...

Is internal SRAM bufferable or not?

Posted on September 04, 2017 at 09:44Hi.I have enabled MPU for different regions with different attrubutes (mainly read only, execute never and no access attributes). For peripherals region I enabled also bufferable attribute (MPU overrides global w...

matic by Associate III
  • 827 Views
  • 0 replies
  • 0 kudos

Creating narrow pulses with STM32F051R8T6 discovery

Posted on September 04, 2017 at 09:19Hi everyoneI'm on a project where i need to create 300 us pulses every 1s so i need 100000 samples on my DAC, but the RAM is not enough to handle with that number of samples. The thing is the pulse information is...