cancel
Showing results for 
Search instead for 
Did you mean: 

transformer stm32f407

gajraj
Associate II
Posted on May 05, 2017 at 08:07

Dear All,

I am  looking for some support in verifying our transformer design as i am  having some trouble in generating the output and i have doubts on the transformers we already have.

> Processor used : STM32F407

> Use case : 48 V DC on the transformer primary is switched by the controller to generate 1600 V Peak to Peak output on the secondary in 160KHz frequency.

> Issue : When the transformer is loaded, the clock of the STM controller changes and there seems to be some disturbance to the power section too.

> When the primary voltage is reduced from 48V to a lessor voltage like 5V-12V, depending on the board, this works as expected with lessor output P2P in the secondary.

Please help me to resolve the issue.

Thanks

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0