cancel
Showing results for 
Search instead for 
Did you mean: 

how can i use DMA?

sunwoo lee
Associate II
Posted on March 30, 2017 at 10:37

i have been stm32F303VDT chip

i use DAM with ADC3 ,4 with Trigger tim2 channel 3

Perfectly done

but I used timer2 so I must change trigger timer 3 .

so  i  changed timer 3 channel 4 but It is not executed.

The procedure is start DMA  next timer Start

HAL_ADC_Start_DMA(&hadc3, (uint32_t*) ADC_I_Result, ADC_NUM);

HAL_ADC_Start_DMA(&hadc4, (uint32_t*) ADC_Q_Result, ADC_NUM);

HAL_TIM_PWM_Start (&htim3, TIM_CHANNEL_4);

why can i used it?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0