STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART receive from ST-Link VCP not working

Posted on March 23, 2017 at 21:32Hi! I'm trying to send some data (or string or anything) from the computer to a Nucleo-64 board, with no luck at all. I can easily retarget the printf and is working perfectly, but it is receiving nothing from the co...

Resolved! How accurate should the PWM input on a Nucleo32L031 be?

Posted on September 04, 2017 at 22:25Hi Folks,I'm relatively new to the STM32 universe so please the giggling to a minimum.I set up the TIM21 to output a 60Hz signal and with an ON time of 3000 ticks x 32 x 1/8MHz = 12.0mshtim21.Instance = TIM21;hti...

STEVAL-IDI004V2

Posted on March 01, 2017 at 15:43Hey folks,I have a http://www.st.com/en/evaluation-tools/steval-idi004v2.html that I will be testing out soon. However, the package didn't come with a wall adapter. The manual says to use a 5V/1A wall adapter. The ba...

Stm32L476 Fatfs using DMA mode

Posted on July 25, 2017 at 16:28Stm32L476 Fatfs using DMA mode https://community.st.com/tags♯/?tags=stm32l476 https://community.st.com/tags♯/?tags=sdmmc%20dma%20stm32l4 https://community.st.com/tags♯/?tags=dma https://community.st.com/tags♯/?tags=sd...

STM32 F103xx HAL UART echo

Posted on August 29, 2017 at 18:15 I am trying to implement a simple echo program using the HAL drivers. Here is my code #include 'stm32f1xx.h' #include 'stm32f1xx_hal.h' #include 'stm32f1xx_hal_conf.h' void Error_Handler(void); void SystemClo...

Tom Eaton by Associate II
  • 4251 Views
  • 6 replies
  • 0 kudos

VDDA and PA2 ADC measurements

Posted on August 30, 2017 at 15:48Hello,I work on a STM32L151CCU6 and I need your help.I try to measure VDDA voltage in order to calculate a voltage divider on PA2 (single mode). My two ADC configuration functions are :void MX_ADC_Init(void){  GPIO_...

I want to use stm32l496 ADC in a differential mode.

Posted on September 04, 2017 at 12:28I want to use stm32l496 ADC in a differential mode. What will the data of the conversion case, if the VINN is greater than the VINP? Will I get a range of output data changes from -4095 to +4095 when VINN changes...

STM32F1xx I2C Receive with HAL

Posted on September 04, 2017 at 17:54 I am trying to interface with an ADS1015 using an STM32F I am having problems reading two bytes from the ADS1 The first byte is received perfectly, but the second byte is exactly the same as the first byte wh...

Tom Eaton by Associate II
  • 1143 Views
  • 0 replies
  • 0 kudos