STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to start ADC in the STM32F746 Discovery Demo?

Posted on September 11, 2017 at 20:28I have modified the demo code to my needs but now I would like to use ADC converter too. I can't find a suitable example for plain ADC(, not Audio ADC). PF10, that is ADC3_IN8, seems to be free and connected to a...

LMI2 by Lead
  • 673 Views
  • 0 replies
  • 0 kudos

SysTick , I dont understand whats happening.

Posted on September 11, 2017 at 17:17Hi,   I am still working my way through the STM32 , and decided to  move away from CubeMX, to use the registers.  I have started by writing the following just to get the systick to work. Im not really interested ...

Can this be an issue with CubeMX?

Posted on April 07, 2017 at 16:42Hi   I am beginning to wonder if this is an issue with CubeMX? I recently posted an issue I am having below on the ADC of the STM32L073 chip. Its a small application created with CubeMX and have checked it many times...

Wifi Module interfacing

Posted on September 11, 2017 at 14:21Hello People ,Is it possible to Interface  wifi module(SPWFxx)  to  STM32Fx  Eval board directly without Nucleo or Extension boards ?regards,Rohith#stm32-mcu-evaluation-board #wifi-module

STM32F031 low voltage reset - bootloader boot0 pin

Posted on September 09, 2017 at 00:02I have two micros communicating over SPI bus, one is a STM32F031 running application code.  I can interrogate the STM32F031 for its firmware version and if it is not the correct version I power off its 3.3 volts,...

STM32F302xC PA11

Posted on September 11, 2017 at 17:39Dear All,I need to use TIM1 to generate 4 PWM signals, hence I want to use CH1, CH2, CH3, CH4.I also need to use USB for firmware upgrade.Since on PA11 there are both TIM1 CH4 and USB-DM, I don't know how to rema...

sirpak by Associate II
  • 947 Views
  • 2 replies
  • 0 kudos

STM32F071RB stdperiph_lib support ?

Posted on September 11, 2017 at 14:09Hey,does someone use stdperiph_lib V1.5 in combination with stm32f071rb ?Just read in the changelog that it was updated in Dec. 2015: Add support of the STM32F070xB, STM32F070x6 and STM32F030xC  devices.But did ...

RM0351 RTC wakeup

Posted on September 10, 2017 at 16:20In the STM32L4x5/4x6 reference manual (and some other manuals too, like RM0090) the figure 374 shows that the RTC wakeup timer can be clocked with ck_apre, but the description of RTC_CR says that the alternate in...

STM32H743I-EVAL

Posted on September 10, 2017 at 08:32Hi,where are the sch or list of this EVAL board 'Free Pins' for GPIO usage,in sch file MB1246 , sheet: Extension Connectors the connectors are drown without listing which port-pin is free and which is used!regard...