cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429IGT SDRAM Read/Write

Ivan Klochkov
Associate
Posted on May 22, 2017 at 14:44

Hi all,

I've got a board with IS45S16400J SDRAM connected to MCU, FMC bank 2. I'm entering data via UART and write it to SDRAM, then I'm reading it and sending back data.

Received data looks kinda strange, the first 8 bytes are the one I was sending but there is happen to be another 32 bytes with random numbers. Then I'm keep receiving those 40 bytes but this time the first 8 are zeroes. Here's loop function (both Rx and Tx buffers are 8 bytes):

  while (1)

  {

HAL_UART_Receive_IT(&huart1, RxBuff, sizeof(RxBuff));

        if(huart1.RxXferCount == 0) {

HAL_SDRAM_Write_8b(&hsdram1, &addr, RxBuff, sizeof(RxBuff));

HAL_SDRAM_Read_8b(&hsdram1, &addr, TxBuff, sizeof(TxBuff));    

HAL_UART_Transmit_IT(&huart1, TxBuff, sizeof(TxBuff));               

        }

  }

The other thing is that I don't actually know what address in HAL_SDRAM_Write/Read should be. Is that offset from bank address or bank address (0xD0000000) with offset? By the way, reference manual says that FMC bank 2 is used by NAND Flash. Does it mean my SDRAM connected incorrectly and I can't use it?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 22, 2017 at 16:38

There is not consistent naming, as I recall the pins refer to Bank0 and Bank1

Look for HAL examples under the Cube install for the EVAL and DISCO boards, should be examples of the 0xC0000000 and 0xD0000000 configurations/use cases

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..