cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F207 standby mode

guenniause
Associate II
Posted on May 22, 2017 at 10:59

Hello,

I'm using STM32F207 with external USB-PHY in device mode.

I want to enter standby mode by SuspendCallback of USB. Because it is not possible to wakeup the STM32 by interrupt (ResumeCallback), I want to use the wakeup pin.

It is possible to use the output pin of external PHY (USB3300, signal D3) for wakeup?

Thanks,

Guenter

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User
Posted on May 22, 2017 at 11:07

RM0033:

The microcontroller exits Standby mode when an external Reset (NRST pin), an IWDG

Reset, a rising edge on WKUP pin, an RTC alarm, a tamper event, or a time stamp event is

detected.