STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem to reach high Frequency on GPIO

Posted on August 25, 2017 at 16:34Hi,i'm using stm32 nucleo board. The oscillator is configured to 32MHz speed.Now, if i use the easy following code in the main:while(1){   HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, 1);    HAL_GPIO_WritePin(LD2_GPIO_...

Lex Trc by Associate II
  • 2114 Views
  • 5 replies
  • 0 kudos

ADC single channel

Posted on September 12, 2017 at 13:03Hi,i'm using Nucleo STM32L053R8 board. How can i read single ADC channel selecting manually avery oneof the 2 channel anabled?Thanks

Lex Trc by Associate II
  • 582 Views
  • 0 replies
  • 0 kudos

STM32F303VCT7 FIT

Posted on September 08, 2017 at 19:22I need the Failure in Time (FIT) number and test conditions for the STM32F303VCT7.

The mouse doesn't work with demonstration examples

Posted on September 10, 2017 at 09:30I have DiscoveryF407VGt6 board, I did try  both of 'STM32F4-Discovery_FW_V1.1.0' and 'en.stm32cubef4' demonstration examples. LEDs work fine by both examples, but there is no mouse action at all!

m m by Associate II
  • 1469 Views
  • 2 replies
  • 0 kudos

Resolved! OLED SSD1322 don't Work

Posted on August 03, 2017 at 09:44 Hi everyone, ì'm trying to use te OLED MCOT256064BA-WM with the SSD1322 Driver. Is so frustrating to be in the situation that the code seems really correct at least , but the OLED don't still Work. I need H...

How to configure linker file in the IAR workbench

Posted on September 12, 2017 at 07:32Hi,Related to https://community.st.com/0D50X00009Xke1tSAB  question, I want to know how we can change Flash origin  address and interrupt vector table base address in IAR work bench?  where we can set desire loca...

Flash erasing using Flash loader demonstration

Posted on September 12, 2017 at 07:02Hi,We are using STM32F101R8T6 controller, we want to erase and load particular flash pages using Flash loader demonstration application. How we can configure the origin of the Flash erasing and writing in the app...

Getting an error compiling lwip/eth/freertos

Posted on September 12, 2017 at 02:21I'm working on an STM32 project for someone else.  Trying to get LWIP/ethernet working.  They are using freertos.  They even said that they got it working at some point to test the hardware.  I found where some f...

Alan K by Associate
  • 589 Views
  • 0 replies
  • 0 kudos