STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPL: NVIC_Init() illogical if not enabling interrupt.

Posted on September 13, 2017 at 14:09I just found this out on electronics stackexchange:If you set the struct member NVIC_IRQChannelCmd = DISABLE, calling NVIC_Init() will do nothing to set the interrupt priority and sub-priority. If you want the in...

Resolved! STM32CubeMX bad macro generation (bug)

Posted on December 24, 2016 at 15:15 I use STM32CubeMX v4.0. It generates MX_Device.h file for configuring CMSIS-Drivers. I found that there are some macroses use hyphen symbol, which is not allowed: /*-------------------------------- SYS ----...

Eugene S. by Associate III
  • 1558 Views
  • 6 replies
  • 0 kudos

STM32F446 MCO2 from I2SPLL

Posted on September 13, 2017 at 12:38There's no source of PLLI2S signal mentioned anywhere else on the schematics, nor elsewhere in RM0360 (although the string occurs quite often as it's the name of the PLLI2S sub-module).My personal guess is, that ...

0690X000006086bQAA.png 0690X00000607t0QAA.png 0690X000006086lQAA.png

2 Timers use with stm32F746BG

Posted on September 05, 2017 at 04:58Hello, I use MDK-Lite 5.23 uVision / stm32F746BG. I work with two timer interrupts at the same moment: TIM1_UP_TIM10_IRQHandler(void) + TIM2_IRQHandler(void) + program code at the main() function  void TIM1_UP_TI...

IR diode connection

Posted on September 13, 2017 at 11:35The following circuit was pointed out on a local electronics forum:I mean, it *may* work, under certain circumstances... nonsense nevertheless.One of the comments was, that it nicely complements Cube... ;)JW

0690X00000608COQAY.png

STM32L496 USART1 RX crash @ 1.8V IO

Posted on September 12, 2017 at 10:50Dear community.I have a very interesting issue - I am working on STM32L496 Nucleo board and working with USART1.  Everything works fine there with USART1 receive/transmitting in INT mode.  (Nucleo runs 3.3v with ...

john chen by Associate II
  • 3135 Views
  • 6 replies
  • 0 kudos