cancel
Showing results for 
Search instead for 
Did you mean: 

SWD EMC issues (pullup SWDIO)

ingwmeier
Senior
Posted on May 18, 2017 at 11:22

AN2586 (Getting started with STM32F10xxx hardware development) recommends

JTMS/SWDIO: Internal pull-up

TCK/SWCLK: Internal pull-down

in an older STM32F100 Project where we had some field issues probably due to EMC (serial interface 3 seems to stop working after a few days or weeks), I realised, that through the use of the standard peripheral library both pins are set to pull-down**. After soldering a 10k pull up to the SWDIO, the problems seemed to stop to occur.

Has anyone experienced similar issues?

BTW the PCB traces to the debug interface are only about 2cm long, GND plane on other side of the PCB.

regards

Werner

** this is shown when you observe GPIOA CNF13 / 14 through the debugger, but I just did a measurement with a DMM, where the correct Pullup on SWDIO and Pulldown to SWCLK can be confirmed

#swd-pullup/pulldown
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0