STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F3 ADC fully differential errata

Posted on September 30, 2017 at 01:06Having some trouble with a fully-differential signal driven directly into STM32F303 setup for differential mode.  There is an errata about common-mode voltage having to be within 10% of center which may or may no...

STM32L43x Nucleo code without HAL

Posted on September 29, 2017 at 21:08Hi   I want to use only the STM32L432 LL drivers by  defining the label USE_FULL_LL_DRIVER. Does anyone have example codes for the blocks like SPI using only drivers and not the HAL?.... Please help.RegardsBala

Resolved! STM32L051 Port PH1 Initialization Error

Posted on September 29, 2017 at 00:23I used STM32CubeMX to generate code for a STM32L051R8xx microcomputer.  All I/O ports initialize correctly except PH1.  If I delete the PH1 initialization code, the program executes correctly.  With the PH1 code ...

[OTG] Endpoint disable in 'F4 and 'L4

Posted on September 29, 2017 at 15:26This question is aimed at those in ST who are deeply familiar with the Synopsys OTG core in its various incarnations.The USB endpoint disable procedures as described in 'F4 and 'L4 RMs are very different; the 'F4...

Initialize STM32f407 Ethernet without using libraries

Posted on September 21, 2017 at 17:03Hi.Is there any procedure available that shows the steps involved in initializing the Ethernet. The cube code generated uses libraries like HAL. I would like to do this without using these libraries. Is there a p...

STM32 L452 : Programming using SWD interface

Posted on September 29, 2017 at 07:03Hello everyone,I am working with STM32 L452 microcontroller. I'm trying to program this using SWD interface on ST link debugger of the Nucleo board. I am powering the L452 MCU via two different methods :1) Using ...

0690X00000608NSQAY.png

Equivalent part

Posted on September 29, 2017 at 07:05Please share the equivalent STM32 ultra low power MCU for the below requirement: Flash Memory size [KB] 128 SRAM size [KB] 8 Speed [MHz] 32 DMA controller Yes Communication Peripherals [UART, SPI,I2C]:3 - UART, ...

PK K by Associate
  • 1020 Views
  • 1 replies
  • 0 kudos