STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F070RBT6 periodic wake-up timer

Posted on October 03, 2017 at 13:12On this site: http://www.st.com/en/microcontrollers/stm32f070rb.html it says that this microcontroller has aCalendar RTC with alarm and periodic wakeup from Stop/Standby. However I don't seem to get the periodic wa...

rwa by Associate
  • 585 Views
  • 0 replies
  • 0 kudos

Resolved! PWM TIM4 4KHz 50% Duty Cycle

Posted on October 03, 2017 at 09:09The original post was too long to process during our migration. Please click on the attachment to read the original post.

GPIO - DMA Peripheral-to-Memory

Posted on February 20, 2017 at 11:43Hi,I'm trying to realize a communication between an external ADC with a parallel interface and a STM32F429 via DMA. Therefore the clock-out signal, provided by the ADC (which indicades the new data is ready, at a ...

Skadi F by Associate II
  • 2483 Views
  • 3 replies
  • 0 kudos

DMA Memory-to-Peripheral Clock

Posted on May 09, 2015 at 20:26Hi, I'm trying to set DMA2 to do a Memory-to-Peripheral trasfer from memory to GPIOB. But now, I'm stuck with a problem since I want to configure the DMA transfer speed to 1/8 of the Bus clock(168Mhz). Is there any way...

pedro by Associate II
  • 1744 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F030 UART problem

Posted on September 28, 2017 at 17:58Hi all,I'm trying to send an HTTP message through Ethernet interface using a WIFI external device. For this, I use HAL_UART functions as shown:HAL_UART_Transmit(huart, messageTX,lengthOfmessage, timeoutTX);UART h...

STM32f030 RTC interface

Posted on October 02, 2017 at 19:32Hi all,I'm trying to work with STM32f030 RTC internal to save UTC calendar.I have included in my FW application the followings functions:- MX_RTC_Init();- Enable RTC interface in 'stm32f00x_hal_conf.c'- Defined RTC...

[OTG + documentation] global NAK clear

Posted on August 28, 2017 at 16:44More.The description of global NAKclearing for both IN and OUT is a mess reoccurring in several places - in the description of four set/clear bits in DCTL, in the narrative in several subchapters of Operational mode...

Configure CAN to receive in both FIFOs

Posted on June 09, 2016 at 10:58 Hello there, I am using STM32F4. I am trying to configure can peripheral the way that when messages are received, they pass through 2 filters. If filter 0 matches they go to FIFO0, if filter 1 matches they sh...

SD card support for X-NUCLEO-IDW04A1 (SPWF04SA) ?

Posted on October 02, 2017 at 06:57Looking for SD card software support for X-NUCLEO-IDW04A1. The board has an SD Card  socket on a secondary SPI interface from the SPWF04SA module, but I cannot locate any software to support reading or writing to t...