cancel
Showing results for 
Search instead for 
Did you mean: 

Keil assembly for stm32f4

eittinfo
Associate II
Posted on June 12, 2017 at 18:53

hi everybody

i have a assembly program and want to use it in my project . but keil don't compile this directly. i don't have enough knowledge to correct and convert code to keil could compile this code. pls help me microcontroller in my project is stm32f4 family tnx alot

.syntax unified
#ifdef __ARM_PCS_VFP
@ High-throughput block transfer using the FPU register set as a 128-byte
@ buffer.
@
@ This implementation exploits the IT Folding feature of the Cortex-M4.
@ An IT instruction following a 16-bit Thumb instruction, when both are
@ aligned into a 32-bit memory word, takes no additional cycles to issue.
@
@ Arguments:
@ r0 source address
@ r1 destination address
@ r2 number of words to transfer.
.section .ramcode,'ax',%progbits
.balign 4
.global _Z10copy_wordsPKmPmm
.thumb_func
_Z10copy_wordsPKmPmm:
@ Name our registers.
src .req r0
dst .req r1
count .req r2
@ The caller may have been using floating point.
@ Save the callee-save portion of the register file.
vpush {s16 - s31} @ 17
@ 'Warm up' the transfer engine, which wants to operate in units of
@ 128 bytes, by making smaller transfers until count a multiple of 
@ Special-case the single word transfer; the macro below won't work.
lsrs.n count, #1 @ 1
itt cs @ 0 (aligned)
vldmcs.32 src!, {s0} @ 2
vstmcs.32 dst!, {s0} @ 2
@ Transfer n+1 words.
.macro XFER n @ 5 + 2*n
lsrs.n count, #1 @ 1
itt cs @ 0 (aligned)
vldmcs.32 src!, {s0 - s\n} @ 1+1+n
vstmcs.32 dst!, {s0 - s\n} @ 1+1+n
.endm
XFER 1 @ 7
XFER 3 @ 11
XFER 7 @ 19
XFER 15 @ 35
@ Handle the case where we've been asked to transfer <32 words.
@ In such a case, count will now be zero, and the Z flag will still
@ be set from the last XFER.
@
@ Force the branch to use a 32-bit instruction to preserve alignment
@ of the loop branch below; this saves a cycle per time that branch
@ is taken.
@
@ Note that the target of this branch (at 1 below) is also aligned,
@ saving a cycle on the rare escape path.
beq.w 1f @ 1 (n.t.)
@ All warmed up, transfer in units of 128 bytes.
0: vldm.32 src!, {s0 - s31} @ 33
vstm.32 dst!, {s0 - s31} @ 33
subs.n count, #1 @ 1
bne.n 0b @ ~3 (taken)
@ Restore FPU state.
1: vpop {s16 - s31} @ 17
bx lr @ 1-3??
#else
#error copy_words is not available for your architecture.
#endif�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on June 13, 2017 at 05:11

; .s built using FPU support, ie --cpu Cortex-M4.fp
; High-throughput block transfer using the FPU register set as a 128-byte
; buffer.
;
; This implementation exploits the IT Folding feature of the Cortex-M4.
; An IT instruction following a 16-bit Thumb instruction, when both are
; aligned into a 32-bit memory word, takes no additional cycles to issue.
;
; Arguments:
; r0 source address
; r1 destination address
; r2 number of words to transfer.
_Z10copy_wordsPKmPmm PROC
 EXPORT _Z10copy_wordsPKmPmm
 ; The caller may have been using floating point.
 ; Save the callee-save portion of the register file.
 vpush {s16 - s31} ; 17
 ; 'Warm up' the transfer engine, which wants to operate in units of
 ; 128 bytes, by making smaller transfers until count a multiple of 
 lsrs.n r2, #1 ; 1
 itt cs ; 0 (aligned)
 vldmcs.32 r0!, {s0} ; 2
 vstmcs.32 r1!, {s0} ; 2
 lsrs.n r2, #1 ; 1
 itt cs ; 0 (aligned)
 vldmcs.32 r0!, {s0 - s1} ; 1+1+1
 vstmcs.32 r1!, {s0 - s1} ; 1+1+1
 lsrs.n r2, #1 ; 1
 itt cs ; 0 (aligned)
 vldmcs.32 r0!, {s0 - s3} ; 1+1+3
 vstmcs.32 r1!, {s0 - s3} ; 1+1+3
 lsrs.n r2, #1 ; 1
 itt cs ; 0 (aligned)
 vldmcs.32 r0!, {s0 - s7} ; 1+1+7
 vstmcs.32 r1!, {s0 - s7} ; 1+1+7
 lsrs.n r2, #1 ; 1
 itt cs ; 0 (aligned)
 vldmcs.32 r0!, {s0 - s15} ; 1+1+15
 vstmcs.32 r1!, {s0 - s15} ; 1+1+15
 ; Handle the case where we've been asked to transfer <32 words.
 ; In such a case, count will now be zero, and the Z flag will still
 ; be set from the last XFER.
 ;
 ; Force the branch to use a 32-bit instruction to preserve alignment
 ; of the loop branch below; this saves a cycle per time that branch
 ; is taken.
 ;
 ; Note that the target of this branch (at 1 below) is also aligned,
 ; saving a cycle on the rare escape path.
 beq.n z1 ; 1 (n.t.)
 ; All warmed up, transfer in units of 128 bytes.
z0 vldm.32 r0!, {s0 - s31} ; 33
 vstm.32 r1!, {s0 - s31} ; 33
 subs.n r2, #1 ; 1
 bne.n z0 ; ~3 (taken)
 ; Restore FPU state.
z1 vpop {s16 - s31} ; 17
 bx lr ; 1-3??
 ENDP ; _Z10copy_wordsPKmPmm
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..