STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DAC specification 8-10bit mode?

Posted on October 04, 2017 at 04:21STM32F4xx1: Do 8bit DAC mode have same specifications as the 10bit mode?2: The 3.3V / 1.5MOhm = 2.2 µA load for 1% accuracy as spec'ed in manual is for internal    buffer off , i had assumed no load at all would g...

Minimum input voltage for stm32f0

Posted on October 03, 2017 at 09:56Hello ST community,What if I provide 2.8V as a Vcc to STM32F0? Does it behave properly?Yes, I have checked input voltage range is 2.4V to 3.6V, still wanted to confirm with you because usually we provide 3.3V to su...

deokar by Associate II
  • 2486 Views
  • 3 replies
  • 0 kudos

Understanding interruptions

Posted on October 03, 2017 at 17:54Hi.I am currently working with a STM32L476 Discovery board.I just want to start an interruption handler with a basic timer, but I am facing an issue.I would like to toggle a LED from the board when the timer is res...

azer asd by Associate II
  • 1557 Views
  • 2 replies
  • 0 kudos

STM32F103 Loss RTC Date when RESET

Posted on August 30, 2017 at 11:18Hello friendsi using STM32CubeMX 4.2.2 & Firmware F103 v1.6 , MCU = STM32F103ZET6I set the time and date in RTC When micro resets I miss the date but time is still rightHow do I fix this problem?Thank,

Pedram by Associate III
  • 2835 Views
  • 6 replies
  • 0 kudos

Resolved! STM32F7 Clock unable to reach 216 MHz

Posted on April 11, 2017 at 16:03 Hi, I'm facing an issue with a new project I'm working on, I just received a custom board based on a STM32F746VGT6 MCU, the MCU wasn't able to run my base program, (generated via MXCube), so I started changing...

emwin Hello world

Posted on December 26, 2016 at 18:54hi.i work on emwin library. in first hello world projectstm32cubef1\STM32Cube_FW_F1_V1.2.0\Projects\STM3210C_EVAL\Applications\STemWin\STemWin_HelloWorldmy code is :HAL_Init(); SystemClock_Config(); BSP_Config();...

dav ABA by Associate II
  • 1072 Views
  • 3 replies
  • 0 kudos