STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F030 was reconfigured by himself - help

Posted on October 03, 2017 at 13:32Hi community,I need help again. I have a problem with my stm32f030RCT6 program. Yesterday I programmed this MCU and today morning a saw problem. Problem is with reconfiguring rcc settings. MCU was programmed with P...

Arm-Gcc MakeFile Windows

Posted on October 04, 2017 at 11:55Simply I am trying to program my stm32f4 discovery without any ide.Another word I want to use  make command on the terminal in Windows.I know this makefile wrote for macos I cant convert the code working under  Win...

USB pull up USB_FS_DP line

Posted on February 03, 2017 at 09:31I use ''USB Device'' on STM.My STM32F401 has USB OTG so it means that it can pull up USB_FS_DP data line without pull up resistor .But I can't find a way how to do it, please help me

0690X00000606EDQAY.png

audio weaver startup problem on Windows 10

Posted on October 04, 2017 at 15:50I installed audio weaver ''Audio_Weaver_Designer_6.17.06_STMicro'' on Windows 10, 64 bit. I actually installed and uninstalled multiple times, thinking the installation failed.I get the following error on startup. ...

0690X00000608TtQAI.png

STM32F302RBT6 compatible with STM32F302R8T6

Posted on September 19, 2017 at 23:27Hi,We are using the device STM32F302R8T6 on our current design. Can I replace this part with STM32F302RBT6 without making firmware changes? I checked on datasheet and found STM32F302RBT6 has everything what STM32...

stm32f373 sdadc switching configuration

Posted on October 04, 2017 at 13:01 Hello everyone! I'm working on the project with an STM32F373 microprocessor. I'm using all three SDADC-s simultaneously. SDADC3 works constantly in Injected scan mode with frequency 16,66kHz. SDADC1 and SD...

HAL_ERROR in HAL_RCC_OscConfig()

Posted on September 29, 2017 at 18:13Hi all!I have an STM32L0 using the HSI to clock at 6MHz, and a LSE for the RTC.Devices goes to sleep (STOP mode) and wakes up just fine.But if I activate the RTC Alarm A interrupt, while restoring clocks I get a ...

STM32F407Z and FatFS. Mounting SD Card issue.

Posted on October 04, 2017 at 10:50Simple problem description: f_mount function from FatFS causes stack problem somethere is parallel tasks in FreeRTOS.More detailed description:We have a project in which we use the processor STM32F407Z and we have ...

Oleg M by Associate
  • 702 Views
  • 0 replies
  • 0 kudos

STM32L4 TIM2 Configuration for Infrared Receiver

Posted on October 04, 2017 at 09:39Dear community,Below are my configuration to capture infrared signals from the TIM2 CH1. Can I get confirmation that I may use these configuration for my purpose;Best Regards,Mete#receiver #stm32l4 #pwm #tim2 #inpu...

0690X00000608T5QAI.png 0690X00000608TFQAY.png