STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F334 HAL DMA ADC Scan conversion not working

Posted on October 09, 2017 at 20:26Hello. In my project, I use the ADC configured in scan mode, as seen on this screenshot from STM32CubeMX:and the DMA configured as follows:The problem is that I can't get any data transferred from ADC to memory, wh...

0690X00000608XgQAI.png 0690X00000608XRQAY.png
RichardS1 by Associate II
  • 2020 Views
  • 3 replies
  • 0 kudos

How to multiply TIMers outputs?

Posted on October 25, 2017 at 11:43Hello everybody:I would like to multiply the outputs I get from TIM3_PWM (64KHz signal) and TIM4_PWM(8MHz signal) in order to get a new signal.The thing is that I don�t know how to do it and I�m pretty lost. By the...

How to divide my Timer output?

Posted on October 26, 2017 at 11:19Hello:I have set my TIM4 in PWM mode to get a 8MHz signal.Now I need to get a 64KHz signal using the 8MHz signal, but I don�t know how to do it.Also, I will have to change the Duty of the 64KHz signal.Thank you in ...

Resolved! Sending float32 with UART

Posted on January 03, 2017 at 18:47Hi there, recently I was making acustic spectrometer using STM32F4-Discover. In my project im making FFT with 'arm_math' libraries and then I need to send data to PC (with which I'll display it) via UART.After maki...

Tom G by Associate
  • 5535 Views
  • 7 replies
  • 0 kudos

STM32F373 Timer questions

Posted on June 24, 2014 at 16:58Hello,I have a timer performing input capture on one channel. Can I set another channel OF THE SAME TIMER as an output with a frequency double of the captured input signal frequency?-------------I am not 100% clear on...

ing by Associate II
  • 2279 Views
  • 5 replies
  • 0 kudos

CAN -> How to send overload frame?

Posted on August 15, 2017 at 05:00Hi,has anyone ever managed to send a standard CAN overload frame on an stm32?So far, I could only find error handling for incoming frames but no way to send one myself.#can #overload

Can not connect to device

Posted on October 24, 2017 at 08:53Hi, I use ST-Link V2 eumlator and STM32 ST-Link Utility SW to flash STM32F103VE. At the beginning, it can flash for several days. Today it can connect to device(show device information), but can't flash. It show ca...

0690X000006049pQAA.jpg
kent gu by Associate III
  • 1691 Views
  • 4 replies
  • 0 kudos