STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F105RC CAN recviev Message is overwritten

Posted on November 01, 2017 at 07:29Dear all,I meet a problem is the messages what I receive via CAN bus are overwritten.I check the datasheet,if FIFO lock function is �enabled�, the incoming message will be discarded. But the value is also overwrit...

0690X00000608ckQAA.png 0690X00000608ocQAA.png 0690X00000608ohQAA.png

Resolved! CAN with a F070?

Posted on November 06, 2017 at 01:14i saw an example from somebody who said he was interfacing a CAN bus with a STM32F070RB, but that chip doesn't have a CAN interface. Anybody know how this is done?thanx, mike#can-bus #can-communitation #stm-32f07

CONNECTING HC 05 with nucleo 64 board

Posted on November 05, 2017 at 05:40hi all hope you are doing well,I wanna connect HC 05 bluetooth module with stm32f303 using nucleo 64 board but i couldn't find any way to connect it with the nucleo 64 board but i found the various illustration us...

STM32H7 series questions ( LQFP)

Posted on November 04, 2017 at 16:24Dear *,I have some questions about the STM32H7 series:1) As i see the MCU can work from 1.6V to 3.5V power supply. a) if i set the VDD to 1.8V than all the I/O and interface pins are 1.8V logic ? b) is it possible...

D Zero by Associate
  • 1053 Views
  • 1 replies
  • 0 kudos

USB CDC Device_Only, re-connect port

Posted on November 05, 2017 at 15:14I'm using STM32F407 Discovery-1, I use USB CDC to send and receive data from terminal. Everything ok but issue that I need re-connect port to transmit and receive data, but i remember that when i used STM32F407 Di...

tan loi by Associate II
  • 696 Views
  • 0 replies
  • 0 kudos

Problem bypassing data from one UART to another?

Posted on November 04, 2017 at 20:14MCU: STM32F777II, running at 64MHzSource UART: UART4 (DMA Stream configured on both RX,TX), Baud Rate: 9600Destination UART: UART8 (DMA Stream configured only for RX), Baud Rate: 9600I need to bypass data coming o...

STM32F7 SPI HAL Driver very slow

Posted on November 03, 2017 at 16:43Hi, I am using Keil and STM32F769I-Eval board.I try to readout a sensor with an external ADC (AD7980). The signal I try to convert runs with 200kHz.I generate with a timer every 5us an interrupt. With the interrup...

0690X00000608p6QAA.png