2016-01-20 1:16 AM
Hi,
Whenever I regenerate the code using STM32CubeMX the new (re-generated) Keil project has Target/IROM1 Memory Areas overwritten e.g. I usually use RAM area are for IROM1 for debug purposes and the IROM1 is set to: Start: 0x20000000, size:0x1000 After regenerating the code the IROM1 settings are overwritten and now I see: Start: 0x8000000, size:0x10000 Is there any way to make STM32Cube preserve Keil Target/IROM settings? Please note Target/IRAM settings are preserved. It looks like a bug. BogdanSolved! Go to Solution.
2016-04-04 7:43 AM
Hi golab.bogdan,
Thank you for your feedback. The issue has been reported internally.-Syrine-2016-04-03 1:12 AM
The bug is still present in 4.14.0
2016-04-03 1:13 AM
Is there any way to make ST developers aware of this issue?
2016-04-04 7:43 AM
Hi golab.bogdan,
Thank you for your feedback. The issue has been reported internally.-Syrine-2016-05-23 3:06 AM
Hi Syrine,
Unfortunately the issue was NOT fixed in the CubeMX 4.15.0. The IROM setting are still altered after re-generating the project using CubeMX. Thanks, Bogdan2016-11-07 8:47 AM
Hi,
I wonder if there any plans to fix the issue. I see the problem also in 4.17.0, Bogdan2017-02-03 4:50 AM
It seems that the issue is fixed at least in 4.19.
Thank you
Bogdan
2017-06-02 10:23 PM
The same error for STM32F745!!! ver. 4.21.0