STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 PCM 8Khz configration problem

Posted on November 04, 2017 at 08:19Hi:   Can STM32F401's PCM be set as the following formats ?   PCM Slave , FS=8Khz ,BITS=16, Mono ( which means BCLK= 8khz * 16 = 128Khz)      After some tests , i find the PCM can only be used as stereo mode (BCLK...

STM32F7 DMA multiple streams

Posted on November 06, 2017 at 17:03Hello, In my custom design am using a STM32F767BITx. Am using an output compare at 5Mghz to trigger the DMA2 and get data from a gpio Port, in circular mode.Am using the DMA_Stream2 and channel 7, DMA_PERIPH_TO_ME...

stm32f103 software uart

Posted on February 28, 2017 at 13:10how can i configure stm32f103 for software uart implementation, are there any documents, reference manual or source code?thanks in advance.#uart #stm32f103c8t6 #software-uart

kosan by Associate II
  • 5953 Views
  • 15 replies
  • 0 kudos

LWIP IPV6

Posted on May 05, 2016 at 15:14Hi. Is there an example for STM32F7 discovery board with IPV6 use? LWIP declares ipv6 compatibility, but in the application example in CUBEf7 library I don't find ipv6 code. Any ideas? Thanks

gb by Associate
  • 2029 Views
  • 2 replies
  • 0 kudos

USART sometimes lost data

Posted on November 10, 2017 at 10:43Hi all?I am using F413 nucleo to acquir water level datas from aquatrak model 4110.The sensor is 1 Hz and data is fixed length.I use timer 6(1Hz) to process the received datas.But I almost lost one record every 90...

_legacyfs_online_stmicro_images_0690X0000060MwOQAU.png _legacyfs_online_stmicro_images_0690X0000060MwJQAU.png

OpenOCD support for external STLink debugger

Posted on November 05, 2017 at 07:41Hi all,Is anyone using OpenOCD with genuine external STLinkV2 debugger/programmer and STM32L0? Clearly, there is an issue as I have tested multiple units and OpenOCD releases (0.9, 0.10.).The debuggers are fully f...

How to use HAL SPI Library

Posted on November 08, 2017 at 16:02Is it possible to use the HAL slave SPI library to receive an unknown number bytes from the master? I'm convinced I'm missing something since the packet size is rarely known in the projects I work on but for some ...

Konami by Senior II
  • 1947 Views
  • 5 replies
  • 0 kudos

STM32F7 HAL I2C Reading bytes out of sync

Posted on April 25, 2016 at 15:27We're currently talking to a few I2C devices on the same bus using latest STM32F7 HAL drivers.All works fine for a while (minutes or hours) and the bus debug on our scope looks perfect, however, every so often we hav...

AndyJT by Associate III
  • 2321 Views
  • 4 replies
  • 0 kudos